File Descriptor Dispatch#
API and Callbacks for the File Descriptor Dispatch Component.
This plugin provides an API to register a file descriptor and a callback that is called when the select() function notifies the plugin there is data on that file descriptor.
Modules#
sl_zigbee_af_file_descriptor_dispatch_struct_t
API#
sl_zigbee_af_file_descriptor_dispatch_add(sl_zigbee_af_file_descriptor_dispatch_struct_t *dispatchStruct)
sl_zigbee_af_file_descriptor_dispatch_wait_for_events(uint32_t timeoutMs)
bool
sl_zigbee_af_file_descriptor_dispatch_remove(int fileDescriptor)
Enumerations#
enum
SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_NONE = 0x00
SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_READ = 0x01
SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_WRITE = 0x02
SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_EXCEPT = 0x03
SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_MAX
}
Typedefs#
typedef void(*
sl_zigbee_af_file_descriptor_ready_callback_t)(void *data, sl_zigbee_af_file_descriptor_operation_t operation)
Functions#
void
Bad file descriptor.
API Documentation#
sl_zigbee_af_file_descriptor_dispatch_add#
sl_status_t sl_zigbee_af_file_descriptor_dispatch_add (sl_zigbee_af_file_descriptor_dispatch_struct_t * dispatchStruct)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_file_descriptor_dispatch_struct_t * | N/A | dispatchStruct |
sl_zigbee_af_file_descriptor_dispatch_wait_for_events#
sl_status_t sl_zigbee_af_file_descriptor_dispatch_wait_for_events (uint32_t timeoutMs)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | timeoutMs |
sl_zigbee_af_file_descriptor_dispatch_remove#
bool sl_zigbee_af_file_descriptor_dispatch_remove (int fileDescriptor)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int | N/A | fileDescriptor |
Enumeration Documentation#
sl_zigbee_af_file_descriptor_operation_t#
sl_zigbee_af_file_descriptor_operation_t
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_NONE | |
| SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_READ | |
| SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_WRITE | |
| SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_EXCEPT | |
| SL_ZIGBEE_AF_FILE_DESCRIPTOR_OPERATION_MAX | |
Typedef Documentation#
sl_zigbee_af_file_descriptor_ready_callback_t#
typedef void(* sl_zigbee_af_file_descriptor_ready_callback_t) (void *data, sl_zigbee_af_file_descriptor_operation_t operation) )(void *data, sl_zigbee_af_file_descriptor_operation_t operation)
Function Documentation#
sl_zigbee_af_file_descriptor_dispatch_bad_file_descriptor_cb#
void sl_zigbee_af_file_descriptor_dispatch_bad_file_descriptor_cb (int fd)
Bad file descriptor.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int | N/A | fd | The bad file descriptor Ver.: always |
The indicated file descriptor has been detected to be bad. For example, the file descriptor caused an EBADF error on a select() call. The file descriptor will be omitted from subsequent file descriptor polling. The application responsible for the file descriptor should take steps to recover and clean up.