IAS Zone Client#
API and Callbacks for the IAS Zone Cluster Client Component.
An implementation of a client for IAS Zone that configures and keeps track of IAS Zone Servers. It requires extending to handle server notifications that might trigger some behavior on the client (e.g., alarm).
Modules#
Functions#
void
sl_zigbee_ias_client_allow_set_cie_address(bool allow)
API to control the setting of CIE address.
Variable Documentation#
sl_zigbee_af_ias_zone_client_known_servers#
sli_zigbee_ias_zone_device_t sl_zigbee_af_ias_zone_client_known_servers[]
Function Documentation#
sl_zigbee_ias_client_allow_set_cie_address#
void sl_zigbee_ias_client_allow_set_cie_address (bool allow)
API to control the setting of CIE address.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | allow |