Prepayment Client#
API and Callbacks for the Prepayment Cluster Client Component.
This component implements the client-side functionality of the Smart Energy 1.2 Prepayment cluster.
Modules#
API#
void
sl_zigbee_af_prepayment_client_change_payment_mode(sl_802154_short_addr_t nodeId, uint8_t srcEndpoint, uint8_t dstEndpoint, uint32_t providerId, uint32_t issuerEventId, uint32_t implementationDateTime, uint16_t proposedPaymentControlConfiguration, uint32_t cutOffValue)
change prepayment client payment mode
API Documentation#
sl_zigbee_af_prepayment_client_change_payment_mode#
void sl_zigbee_af_prepayment_client_change_payment_mode (sl_802154_short_addr_t nodeId, uint8_t srcEndpoint, uint8_t dstEndpoint, uint32_t providerId, uint32_t issuerEventId, uint32_t implementationDateTime, uint16_t proposedPaymentControlConfiguration, uint32_t cutOffValue)
change prepayment client payment mode
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_short_addr_t | N/A | nodeId | Ver.: always |
| uint8_t | N/A | srcEndpoint | Ver.: always |
| uint8_t | N/A | dstEndpoint | Ver.: always |
| uint32_t | N/A | providerId | Ver.: always |
| uint32_t | N/A | issuerEventId | Ver.: always |
| uint32_t | N/A | implementationDateTime | Ver.: always |
| uint16_t | N/A | proposedPaymentControlConfiguration | Ver.: always |
| uint32_t | N/A | cutOffValue | Ver.: always |