GBZ Message Controller#
API and Callbacks for the GBZ Message Controller Component.
Silicon Labs implementation of a GBZ message controller. This component extracts ZCL commands by parsing the elemental GBZ components of the GBZ message. Processing of encrypted GBZ message is not supported.
Modules#
sl_zigbee_af_gbz_zcl_command_t
sl_zigbee_af_gbz_message_parser_state_t
sli_zigbee_af_gbz_payload_header
sli_zigbee_af_gbz_use_case_specific_component
sl_zigbee_af_gbz_message_creator_result_t
sl_zigbee_af_gbz_message_creator_state_t
API#
Assemble appended ZCL responses into 1 big chunk of memory.
Get the default response byte from the GBZ ZCL Command.
Check the GBZ parser structure for any non-parsed commands.
Clean any resources allocated during the parsing of GBZ message.
Initialize proper parsing states for decoding GBZ messages.
Append a ZCL command to a given GBZ creator structure.
Initialize proper states for construction of GBZ messages.
Return the command size of the given parser structure.
Clean up/free all allocated memory used to store the overall GBZ response.
Get the next available ZCL command from the given GBZ parser structure.
Print out all information retained in a sl_zigbee_af_gbz_zcl_command_t structure.
Indicate whether the ZCL payload will be encrypted.
Enumerations#
Typedefs#
Functions#
Macros#
API Documentation#
sl_zigbee_af_gbz_message_controller_creator_assemble#
sl_zigbee_af_gbz_message_creator_result_t * sl_zigbee_af_gbz_message_controller_creator_assemble (sl_zigbee_af_gbz_message_creator_state_t * state)
Assemble appended ZCL responses into 1 big chunk of memory.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_creator_state_t * | N/A | state |
sl_zigbee_af_gbz_message_controller_get_zcl_default_response#
sl_zigbee_af_status_t sl_zigbee_af_gbz_message_controller_get_zcl_default_response (sl_zigbee_af_gbz_zcl_command_t * cmd)
Get the default response byte from the GBZ ZCL Command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_zcl_command_t * | N/A | cmd | status. |
sl_zigbee_af_gbz_message_controller_has_next_command#
bool sl_zigbee_af_gbz_message_controller_has_next_command (sl_zigbee_af_gbz_message_parser_state_t * state)
Check the GBZ parser structure for any non-parsed commands.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_parser_state_t * | N/A | state | A structure containing the bookkeeping information of parsed GBZ messages. |
sl_zigbee_af_gbz_message_controller_parser_cleanup#
void sl_zigbee_af_gbz_message_controller_parser_cleanup (sl_zigbee_af_gbz_message_parser_state_t * state)
Clean any resources allocated during the parsing of GBZ message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_parser_state_t * | N/A | state | A pre-allocated structure that's updated to hold bookkeeping information of parsed GBZ messages. |
sl_zigbee_af_gbz_message_controller_parser_init#
bool sl_zigbee_af_gbz_message_controller_parser_init (sl_zigbee_af_gbz_message_parser_state_t * state, sl_zigbee_af_gbz_message_type_t type, uint8_t * gbzCommand, uint16_t gbzCommandLength, bool copyGbzCommand, uint16_t messageCode)
Initialize proper parsing states for decoding GBZ messages.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_parser_state_t * | N/A | state | A pre-allocated structure that's updated to hold bookkeeping information for parsing GBZ messages. |
| sl_zigbee_af_gbz_message_type_t | N/A | type | A pointer to GBZ messages. |
| uint8_t * | N/A | gbzCommand | Length of GBZ messages. |
| uint16_t | N/A | gbzCommandLength | A flag to indicate if the parser should be storing the GBZ command locally for parsing. |
| bool | N/A | copyGbzCommand | "Message Code" for the corresponding Non TOM command. |
| uint16_t | N/A | messageCode |
The GBZ message payload and payload length are passed in as arguments. Iterator functions, sl_zigbee_af_gbz_message_controller_has_next_command() and sl_zigbee_af_gbz_message_controller_next_command() are used to iterate through each of the embedded ZCL functions.
sl_zigbee_af_gbz_message_controller_append_command#
uint16_t sl_zigbee_af_gbz_message_controller_append_command (sl_zigbee_af_gbz_message_creator_state_t * state, sl_zigbee_af_gbz_zcl_command_t * zclCmd)
Append a ZCL command to a given GBZ creator structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_creator_state_t * | N/A | state | A pre-allocated structure that's updated to hold bookkeeping information of creating GBZ messages. |
| sl_zigbee_af_gbz_zcl_command_t * | N/A | zclCmd | A structure containing information for new ZCL command. |
Returns
0 - if the appending operation did not succeed else - number of appended bytes.
sl_zigbee_af_gbz_message_controller_creator_init#
uint16_t sl_zigbee_af_gbz_message_controller_creator_init (sl_zigbee_af_gbz_message_creator_state_t * state, sl_zigbee_af_gbz_message_type_t type, uint16_t alertCode, uint32_t timestamp, uint16_t messageCode, uint8_t * gbzCommand, uint16_t gbzCommandLength)
Initialize proper states for construction of GBZ messages.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_creator_state_t * | N/A | state | A pre-allocated structure that will be updated to hold bookkeeping information for creating GBZ messages. |
| sl_zigbee_af_gbz_message_type_t | N/A | type | GBZ payload type: command, response, or alert. |
| uint16_t | N/A | alertCode | When type is alert this field contains the alert code. |
| uint32_t | N/A | timestamp | When type is alert this field contains the UTC when the alert occurred. |
| uint16_t | N/A | messageCode | NULL - if the user wants API to allocate memory to store responses. Otherwise - a pointer to destination buffer for GBZ messages |
| uint8_t * | N/A | gbzCommand | Length of GBZ messages. this argument is ignored if gbzCommand is NULL. |
| uint16_t | N/A | gbzCommandLength |
Depending on the value of the argument (gbzCommand), the creator behaves differently. If a NULL value is passed, the creator assumes you want the API to allocate memory to store the appended responses. Otherwise, the creator uses the provided buffer as the destination for storing responses.
Below is a general flow to make ZCL messages into a GBZ message.
sl_zigbee_af_gbz_message_controller_append_command() - append
sl_zigbee_af_gbz_message_controller_creator_assemble() - assemble result.
sl_zigbee_af_gbz_message_controller_creator_cleanup() - memory clean up
sl_zigbee_af_gbz_message_controller_get_component_size#
uint8_t sl_zigbee_af_gbz_message_controller_get_component_size (sl_zigbee_af_gbz_message_parser_state_t * state)
Return the command size of the given parser structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_parser_state_t * | N/A | state | A structure containing the bookkeeping information of parsed GBZ messages. |
sl_zigbee_af_gbz_message_controller_creator_cleanup#
void sl_zigbee_af_gbz_message_controller_creator_cleanup (sl_zigbee_af_gbz_message_creator_state_t * state)
Clean up/free all allocated memory used to store the overall GBZ response.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_creator_state_t * | N/A | state |
sl_zigbee_af_gbz_message_controller_next_command#
void sl_zigbee_af_gbz_message_controller_next_command (sl_zigbee_af_gbz_message_parser_state_t * state, sl_zigbee_af_gbz_zcl_command_t * gbzZclCommand)
Get the next available ZCL command from the given GBZ parser structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_parser_state_t * | N/A | state | A structure that retains the bookkeeping info of parsing GBZ messages. |
| sl_zigbee_af_gbz_zcl_command_t * | N/A | gbzZclCommand | A pre-allocated buffer that will be modified with the next available ZCL command's information. |
If any payload is encrypted, the decrypted data will overwrite the old data.
sl_zigbee_af_gbz_message_controller_print_command_info#
void sl_zigbee_af_gbz_message_controller_print_command_info (sl_zigbee_af_gbz_zcl_command_t * gbzZclCommand)
Print out all information retained in a sl_zigbee_af_gbz_zcl_command_t structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_zcl_command_t * | N/A | gbzZclCommand |
sl_zigbee_af_gbz_message_controller_get_encrypt_payload_flag#
bool sl_zigbee_af_gbz_message_controller_get_encrypt_payload_flag (sl_zigbee_af_gbz_message_creator_state_t * state, sl_zigbee_af_gbz_zcl_command_t * resp)
Indicate whether the ZCL payload will be encrypted.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_gbz_message_creator_state_t * | N/A | state | |
| sl_zigbee_af_gbz_zcl_command_t * | N/A | resp |
Enumeration Documentation#
sli_zigbee_gbcs_use_case_message_code_t#
sli_zigbee_gbcs_use_case_message_code_t
| Enumerator | |
|---|---|
| GCS06_MESSAGE_CODE | |
| GCS11_MESSAGE_CODE | |
| CS11_MESSAGE_CODE | |
| GCS01a_MESSAGE_CODE | |
| GCS01b_MESSAGE_CODE | |
| GCS05_MESSAGE_CODE | |
| GCS07_MESSAGE_CODE | |
| GCS09_MESSAGE_CODE | |
| GCS13a_MESSAGE_CODE | |
| GCS13b_MESSAGE_CODE | |
| GCS13c_MESSAGE_CODE | |
| GCS14_MESSAGE_CODE | |
| GCS17_MESSAGE_CODE | |
| GCS21d_MESSAGE_CODE | |
| GCS21e_MESSAGE_CODE | |
| GCS21j_MESSAGE_CODE | |
| GCS23_MESSAGE_CODE | |
| GCS25_MESSAGE_CODE | |
| GCS33_MESSAGE_CODE | |
| GCS38_MESSAGE_CODE | |
| GCS44_MESSAGE_CODE | |
| GCS46_MESSAGE_CODE | |
| GCS60_MESSAGE_CODE | |
| CS10a_MESSAGE_CODE | |
| CS10b_MESSAGE_CODE | |
| GCS61_MESSAGE_CODE | |
| GCS16a_MESSAGE_CODE | |
| GCS16b_MESSAGE_CODE | |
| GCS15b_MESSAGE_CODE | |
| GCS15c_MESSAGE_CODE | |
| GCS15d_MESSAGE_CODE | |
| GCS15e_MESSAGE_CODE | |
| GCS21f_MESSAGE_CODE | |
| GCS21b_MESSAGE_CODE | |
| GCS53_MESSAGE_CODE | |
| TEST_ENCRYPTED_MESSAGE_CODE | |
| TEST_MESSAGE_CODE | |
sl_zigbee_af_gbz_extended_header_control_field_t#
sl_zigbee_af_gbz_extended_header_control_field_t
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_GBZ_NOT_LAST_UNENCRYPTED_MESSAGE | |
| SL_ZIGBEE_AF_GBZ_LAST_UNENCRYPTED_MESSAGE | |
| SL_ZIGBEE_AF_GBZ_NOT_LAST_ENCRYPTED_MESSAGE | |
| SL_ZIGBEE_AF_GBZ_LAST_ENCRYPTED_MESSAGE | |
sl_zigbee_af_gbz_message_type_t#
sl_zigbee_af_gbz_message_type_t
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_GBZ_MESSAGE_COMMAND | |
| SL_ZIGBEE_AF_GBZ_MESSAGE_RESPONSE | |
| SL_ZIGBEE_AF_GBZ_MESSAGE_ALERT | |
Typedef Documentation#
sli_zigbee_af_gbz_use_case_specific_component#
typedef struct sli_zigbee_af_gbz_use_case_specific_component sli_zigbee_af_gbz_use_case_specific_component
Function Documentation#
sl_zigbee_af_cluster_specific_command_parse#
sl_zigbee_af_zcl_request_status_t sl_zigbee_af_cluster_specific_command_parse (sl_zigbee_af_cluster_command_t * cmd)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_cluster_command_t * | N/A | cmd |