Tunneling Client#
API and Callbacks for the Tunneling Cluster Client Component.
Silicon Labs implementation of Tunneling client cluster. This component requires extending to integrate the software that processes the tunneled data. Note if the maximum transfer size requires fragmentation, manually include the Fragmentation component and configure it to support the tunnel data size. Additionally, the component uses the address table to communicate with the server, so you must manually configure the address table size so that it accommodates active tunnels managed by this component as well as any other entries created during normal operation.
Modules#
API#
Request a tunneling cluster tunnel with a server.
Transfer data to a server through a tunneling cluster tunnel.
Close a tunneling cluster tunnel.
Clean up a tunneling cluster tunnel.
Macros#
API Documentation#
sl_zigbee_af_tunneling_client_request_tunnel#
sl_zigbee_af_plugin_tunneling_client_status_t sl_zigbee_af_tunneling_client_request_tunnel (sl_802154_short_addr_t server, uint8_t clientEndpoint, uint8_t serverEndpoint, uint8_t protocolId, uint16_t manufacturerCode, bool flowControlSupport)
Request a tunneling cluster tunnel with a server.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_short_addr_t | N/A | server | The network address of the server to which the request will be sent. |
| uint8_t | N/A | clientEndpoint | The local endpoint from which the request will be sent. |
| uint8_t | N/A | serverEndpoint | The remote endpoint to which the request will be sent. |
| uint8_t | N/A | protocolId | The protocol ID of the requested tunnel. |
| uint16_t | N/A | manufacturerCode | The manufacturer code of the requested tunnel. |
| bool | N/A | flowControlSupport | true if flow control support is requested or false if not. Note: flow control is not currently supported by the Tunneling client or server plugins. |
This function requests a tunnel with a server. The tunneling client plugin will look up the long address of the server (using discovery, if necessary), establish a link key with the server, and create an address table entry for the server before sending the request. All future communication using the tunnel will be sent using the address table entry. The plugin will call sl_zigbee_af_tunneling_client_tunnel_opened_cb with the status of the request.
Returns
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_SUCCESS if the request is in process or another sl_zigbee_af_plugin_tunneling_client_status_t otherwise.
sl_zigbee_af_tunneling_client_transfer_data#
sl_zigbee_af_status_t sl_zigbee_af_tunneling_client_transfer_data (uint8_t tunnelIndex, uint8_t * data, uint16_t dataLen)
Transfer data to a server through a tunneling cluster tunnel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | tunnelIndex | The index of the tunnel through which to send data. |
| uint8_t * | N/A | data | The buffer containing the raw octets of data. |
| uint16_t | N/A | dataLen | The length in octets of the data. |
This function transfers data to a server through a tunnel. The tunneling client plugin will send data to the endpoint on the node that is managing the given tunnel.
Returns
SL_ZIGBEE_ZCL_STATUS_SUCCESS Indicates if data was sent, SL_ZIGBEE_ZCL_STATUS_FAILURE if an error occurred, or SL_ZIGBEE_ZCL_STATUS_NOT_FOUND if the tunnel does not exist.
sl_zigbee_af_tunneling_client_close_tunnel#
sl_zigbee_af_status_t sl_zigbee_af_tunneling_client_close_tunnel (uint8_t tunnelIndex)
Close a tunneling cluster tunnel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | tunnelIndex | The index of the tunnel to close. |
This function closes a tunnel. The tunneling client plugin will send the close command to the endpoint on the node that is managing the given tunnel.
Returns
SL_ZIGBEE_ZCL_STATUS_SUCCESS Indicates if the close request was sent, SL_ZIGBEE_ZCL_STATUS_FAILURE if an error occurred, or SL_ZIGBEE_ZCL_STATUS_NOT_FOUND if the tunnel does not exist.
sl_zigbee_af_tunneling_client_cleanup#
void sl_zigbee_af_tunneling_client_cleanup (uint8_t tunnelIndex)
Clean up a tunneling cluster tunnel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | tunnelIndex | The index of the tunnel to clean up. |
This function cleans up all states associated with a tunnel. The tunneling client plugin will not send the close command.