Zigbee Security Manager APIs#
This file describes functionality for Zigbee security features. This includes storing and fetching various keys, as well as invoking crypto operations.
See zigbee_security_manager.h for source code.
Functions#
This routine will initialize a Security Manager context correctly for use in subsequent function calls.
Import a key into storage. Certain keys are indexed, while others are not, as described here.
If context->core_key_type is..
..SL_ZB_SEC_MAN_KEY_TYPE_NETWORK, then context->key_index dictates whether to import the current (active) network key (index 0) or the alternate network key (index 1).
..SL_ZB_SEC_MAN_KEY_TYPE_TC_LINK_WITH_TIMEOUT, then context->eui64 must be set. context->key_index is unused.
..SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK, then context->key_index determines which index in the persisted key table that the entry should be stored to. context->eui64 must also be set. If context->key_index is 0xFF, a suitable key index will be found (either one storing an existing key with address of context->eui64, or an open entry), and context->key_index will be updated with where the entry was stored.
..SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_PROXY_TABLE_KEY or SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_SINK_TABLE_KEY, then context->key_index dictates which key entry to import. These Green Power keys are indexed keys, and there are SL_ZIGBEE_GP_PROXY_TABLE_SIZE/SL_ZIGBEE_GP_SINK_TABLE_SIZE many of them.
For all other key types, both context->key_index and context->eui64 are not used.
Import a link key, or SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK key, into storage.
Export an APS link key by index.
Search through the Key table to find an entry that has the same EUI address as the passed value. If NULL is passed in for the address then it finds the first unused entry and sets the index in the context. It is valid to pass in NULL to plaintext_key or key_data in case the index of the referenced key is desired but not its value or other metadata.
Return true if a link key is available for securing messages sent to the remote device. This function simply checks for the existence of a key, it doesn't care if the key is authorized or not. This function searches in a few different places, and it may always return true if certain bits/policies are set. E.g: On trust center, this function always returns true if hashed link keys are used (SL_ZIGBEE_TRUST_CENTER_USES_HASHED_LINK_KEY), or if SL_ZIGBEE_TRUST_CENTER_GLOBAL_LINK_KEY is set.
Add a transient or temporary key entry to key storage. A key entry added with this API is timed out after SL_ZIGBEE_TRANSIENT_KEY_TIMEOUT_S seconds, unless the key entry was added using the Network Creator Security component, in which case the key will time out after the longer between ::SL_ZIGBEE_AF_PLUGIN_NETWORK_CREATOR_SECURITY_NETWORK_OPEN_TIME_S seconds and SL_ZIGBEE_TRANSIENT_KEY_TIMEOUT_S seconds.
Search for a transient, or temporary, key entry from key storage by EUI.
Search for a transient, or temporary, key entry from key storage by key index.
Export a key from storage. Certain keys are indexed, while others are not, as described here.
If context->core_key_type is..
..SL_ZB_SEC_MAN_KEY_TYPE_NETWORK, then context->key_index dictates whether to export the current (active) network key (index 0) or the alternate network key (index 1).
..SL_ZB_SEC_MAN_KEY_TYPE_TC_LINK, then context->eui64 is checked if context->flags is set to ZB_SEC_MAN_FLAG_EUI_IS_VALID. If the EUI supplied does not match the TC EUI stored on the local device (if it is known), then an error is thrown.
..SL_ZB_SEC_MAN_KEY_TYPE_TC_LINK_WITH_TIMEOUT, then keys may be searched by context->eui64 or context->key_index. context->flags determines how to search (see ::sl_zigbee_sec_man_flags_t).
..SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK, then keys may be searched by context->eui64 or context->key_index. context->flags determines how to search (see ::sl_zigbee_sec_man_flags_t).
..SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_PROXY_TABLE_KEY or SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_SINK_TABLE_KEY, then context->key_index dictates which key entry to export. These Green Power keys are indexed keys, and there are SL_ZIGBEE_GP_PROXY_TABLE_SIZE/SL_ZIGBEE_GP_SINK_TABLE_SIZE many of them.
For all other key types, both context->key_index and context->eui64 are not used.
Search for a transient, or temporary, key and deletes it from key storage. Keys can be searched by EUI or key_index based on context->flags (see ::ZB_SEC_MAN_FLAG_EUI_IS_VALID and ::ZB_SEC_MAN_FLAG_KEY_INDEX_IS_VALID).
Delete the key table entry, or a key of type SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK, from storage. Keys can be searched by EUI or key_index based on context->flags (see ::ZB_SEC_MAN_FLAG_EUI_IS_VALID and ::ZB_SEC_MAN_FLAG_KEY_INDEX_IS_VALID).
Check that the passed key exists and can be successfully loaded. This function does not actually load the context, but only checks that it can be loaded.
Retrieve information about the network key and alternate network key. It will not retrieve the actual network key contents.
Retrieve metadata about an APS key. It does not retrieve the actual key contents.
Delete a key from storage. Certain keys are indexed, while others are not, as described here.
If context->core_key_type is..
..SL_ZB_SEC_MAN_KEY_TYPE_NETWORK, then context->key_index dictates whether to delete the current (active) network key (index 0) or the alternate network key (index 1).
..SL_ZB_SEC_MAN_KEY_TYPE_TC_LINK_WITH_TIMEOUT, then keys may be searched by context->eui64 or context->key_index. context->flags determines how to search (see ::sl_zigbee_sec_man_flags_t).
..SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK, then keys may be searched by context->eui64 or context->key_index. context->flags determines how to search (see ::sl_zigbee_sec_man_flags_t).
Load the specified key into the Security Manager's internal context. Any subsequent crypto operations will be done with that loaded context.
Using a previously set key context, the Security Manager will perform an HMAC (keyed hash) using AES-MMO as the hashing algorithm, and AES-128 for the underlying block encryption.
Encrypt/Decrypt the specified data using AES-CCM with AES-128 and a MIC of the requested length (in * bytes). See documentation for sl_zb_sec_ * man_aes_ccm for information on parameters besides mic_length.
Encrypt/Decrypt the specified data using AES-CCM with AES-128 and a 4-byte MIC.
Perform AES-128 crypto on the specified 16-byte block using a previously loaded context.
Finds the Link Key Table index of the symmetric passphase of the given device EUI64.
Imports the symmetric passphrase to the Link Key Table.
Exports the symmetric passphrase from the Link Key Table.
Updates the device address of a symmetric passphrase entry.
Checks whether a new link key with a device can be stored.
Check whether the key referenced by a given context has a specified value. This API is only compatible with keys that permit the standard Zigbee encryption algorithm and have a core key type that is not SL_ZB_SEC_MAN_KEY_TYPE_INTERNAL.
Macros#
Returns whether a Symmetric Passphrase can be stored.
Function Documentation#
sl_zigbee_sec_man_init_context#
void sl_zigbee_sec_man_init_context (sl_zigbee_sec_man_context_t * context)
This routine will initialize a Security Manager context correctly for use in subsequent function calls.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context |
sl_zigbee_sec_man_import_key#
sl_status_t sl_zigbee_sec_man_import_key (sl_zigbee_sec_man_context_t * context, const sl_zigbee_sec_man_key_t * plaintext_key)
Import a key into storage. Certain keys are indexed, while others are not, as described here.
If context->core_key_type is..
..SL_ZB_SEC_MAN_KEY_TYPE_NETWORK, then context->key_index dictates whether to import the current (active) network key (index 0) or the alternate network key (index 1).
..SL_ZB_SEC_MAN_KEY_TYPE_TC_LINK_WITH_TIMEOUT, then context->eui64 must be set. context->key_index is unused.
..SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK, then context->key_index determines which index in the persisted key table that the entry should be stored to. context->eui64 must also be set. If context->key_index is 0xFF, a suitable key index will be found (either one storing an existing key with address of context->eui64, or an open entry), and context->key_index will be updated with where the entry was stored.
..SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_PROXY_TABLE_KEY or SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_SINK_TABLE_KEY, then context->key_index dictates which key entry to import. These Green Power keys are indexed keys, and there are SL_ZIGBEE_GP_PROXY_TABLE_SIZE/SL_ZIGBEE_GP_SINK_TABLE_SIZE many of them.
For all other key types, both context->key_index and context->eui64 are not used.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context | [IN] The context to set. The context dictates which key type to save, key_index (if applicable) into the relevant key storage, eui64 (if applicable), etc. |
| const sl_zigbee_sec_man_key_t * | N/A | plaintext_key | [IN] The key to import. |
Note
The context->derived_type must be SL_ZB_SEC_MAN_DERIVED_KEY_TYPE_NONE, else, an error will be thrown. Key derivations, which are used in crypto operations, are performed using the sl_zigbee_sec_man_load_key_context routine.
Returns
SL_STATUS_OK upon success, a valid error code otherwise.
sl_zigbee_sec_man_import_link_key#
sl_status_t sl_zigbee_sec_man_import_link_key (uint8_t index, sl_802154_long_addr_t address, sl_zigbee_sec_man_key_t * plaintext_key)
Import a link key, or SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK key, into storage.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | [IN] The index to set or overwrite in the key table for keys of type SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK. If index is set to 0xFF (255), then the key will either overwrite whichever key table entry has an EUI of address (if one exists) or write to the first available key table entry. The index that the key was placed into will not be returned by this API. |
| sl_802154_long_addr_t | N/A | address | [IN] The EUI belonging to the key. |
| sl_zigbee_sec_man_key_t * | N/A | plaintext_key | [IN] A pointer to the key to import. |
Returns
SL_STATUS_OK upon success, a valid error code otherwise.
sl_zigbee_sec_man_export_link_key_by_index#
sl_status_t sl_zigbee_sec_man_export_link_key_by_index (uint8_t index, sl_zigbee_sec_man_context_t * context, sl_zigbee_sec_man_key_t * plaintext_key, sl_zigbee_sec_man_aps_key_metadata_t * key_data)
Export an APS link key by index.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | |
| sl_zigbee_sec_man_context_t * | N/A | context | |
| sl_zigbee_sec_man_key_t * | N/A | plaintext_key | |
| sl_zigbee_sec_man_aps_key_metadata_t * | N/A | key_data |
sl_zigbee_sec_man_export_link_key_by_eui#
sl_status_t sl_zigbee_sec_man_export_link_key_by_eui (sl_802154_long_addr_t eui, sl_zigbee_sec_man_context_t * context, sl_zigbee_sec_man_key_t * plaintext_key, sl_zigbee_sec_man_aps_key_metadata_t * key_data)
Search through the Key table to find an entry that has the same EUI address as the passed value. If NULL is passed in for the address then it finds the first unused entry and sets the index in the context. It is valid to pass in NULL to plaintext_key or key_data in case the index of the referenced key is desired but not its value or other metadata.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_long_addr_t | N/A | eui | |
| sl_zigbee_sec_man_context_t * | N/A | context | |
| sl_zigbee_sec_man_key_t * | N/A | plaintext_key | |
| sl_zigbee_sec_man_aps_key_metadata_t * | N/A | key_data |
sl_zigbee_sec_man_have_link_key#
bool sl_zigbee_sec_man_have_link_key (sl_802154_long_addr_t eui)
Return true if a link key is available for securing messages sent to the remote device. This function simply checks for the existence of a key, it doesn't care if the key is authorized or not. This function searches in a few different places, and it may always return true if certain bits/policies are set. E.g: On trust center, this function always returns true if hashed link keys are used (SL_ZIGBEE_TRUST_CENTER_USES_HASHED_LINK_KEY), or if SL_ZIGBEE_TRUST_CENTER_GLOBAL_LINK_KEY is set.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_long_addr_t | N/A | eui | The long address of some other device in the network. |
Returns
bool Returns true if a link key can be retrieved/computed for securing messages sent to the remote EUI passed as argument. Returns false if a link key is not available for that EUI.
sl_zigbee_sec_man_import_transient_key#
sl_status_t sl_zigbee_sec_man_import_transient_key (sl_802154_long_addr_t eui64, sl_zigbee_sec_man_key_t * plaintext_key)
Add a transient or temporary key entry to key storage. A key entry added with this API is timed out after SL_ZIGBEE_TRANSIENT_KEY_TIMEOUT_S seconds, unless the key entry was added using the Network Creator Security component, in which case the key will time out after the longer between ::SL_ZIGBEE_AF_PLUGIN_NETWORK_CREATOR_SECURITY_NETWORK_OPEN_TIME_S seconds and SL_ZIGBEE_TRANSIENT_KEY_TIMEOUT_S seconds.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_long_addr_t | N/A | eui64 | [IN] An sl_802154_long_addr_t to import. |
| sl_zigbee_sec_man_key_t * | N/A | plaintext_key | [IN] A sl_zigbee_sec_man_key_t* to import. |
Returns
See ::zb_sec_man_import_transient_key for return information.
sl_zigbee_sec_man_export_transient_key_by_eui#
sl_status_t sl_zigbee_sec_man_export_transient_key_by_eui (sl_802154_long_addr_t eui64, sl_zigbee_sec_man_context_t * context, sl_zigbee_sec_man_key_t * plaintext_key, sl_zigbee_sec_man_aps_key_metadata_t * key_data)
Search for a transient, or temporary, key entry from key storage by EUI.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_long_addr_t | N/A | eui64 | [IN] The EUI to search for. |
| sl_zigbee_sec_man_context_t * | N/A | context | [OUT] The context about the key, filled in upon success. |
| sl_zigbee_sec_man_key_t * | N/A | plaintext_key | [OUT] If the security configuration allows for it, filled in with the key contents upon success. |
| sl_zigbee_sec_man_aps_key_metadata_t * | N/A | key_data | [OUT] Filled in with metadata about the key upon success. |
Returns
sl_status_t SL_STATUS_OK upon success, SL_STATUS_NOT_FOUND otherwise.
sl_zigbee_sec_man_export_transient_key_by_index#
sl_status_t sl_zigbee_sec_man_export_transient_key_by_index (uint8_t index, sl_zigbee_sec_man_context_t * context, sl_zigbee_sec_man_key_t * plaintext_key, sl_zigbee_sec_man_aps_key_metadata_t * key_data)
Search for a transient, or temporary, key entry from key storage by key index.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | [IN] The key_index to fetch. |
| sl_zigbee_sec_man_context_t * | N/A | context | [OUT] The context about the key, filled in upon success. |
| sl_zigbee_sec_man_key_t * | N/A | plaintext_key | [OUT] If the security configuration allows for it, filled in with the key contents upon success. |
| sl_zigbee_sec_man_aps_key_metadata_t * | N/A | key_data | [OUT] Filled in with metadata about the key upon success. |
Returns
sl_status_t SL_STATUS_OK upon success, SL_STATUS_NOT_FOUND otherwise.
sl_zigbee_sec_man_export_key#
sl_status_t sl_zigbee_sec_man_export_key (sl_zigbee_sec_man_context_t * context, sl_zigbee_sec_man_key_t * plaintext_key)
Export a key from storage. Certain keys are indexed, while others are not, as described here.
If context->core_key_type is..
..SL_ZB_SEC_MAN_KEY_TYPE_NETWORK, then context->key_index dictates whether to export the current (active) network key (index 0) or the alternate network key (index 1).
..SL_ZB_SEC_MAN_KEY_TYPE_TC_LINK, then context->eui64 is checked if context->flags is set to ZB_SEC_MAN_FLAG_EUI_IS_VALID. If the EUI supplied does not match the TC EUI stored on the local device (if it is known), then an error is thrown.
..SL_ZB_SEC_MAN_KEY_TYPE_TC_LINK_WITH_TIMEOUT, then keys may be searched by context->eui64 or context->key_index. context->flags determines how to search (see ::sl_zigbee_sec_man_flags_t).
..SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK, then keys may be searched by context->eui64 or context->key_index. context->flags determines how to search (see ::sl_zigbee_sec_man_flags_t).
..SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_PROXY_TABLE_KEY or SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_SINK_TABLE_KEY, then context->key_index dictates which key entry to export. These Green Power keys are indexed keys, and there are SL_ZIGBEE_GP_PROXY_TABLE_SIZE/SL_ZIGBEE_GP_SINK_TABLE_SIZE many of them.
For all other key types, both context->key_index and context->eui64 are not used.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context | [IN/OUT] The context to set. The context dictates which key type to export, which key_index (if applicable) into the relevant key storage, which eui64 (if applicable), etc. |
| sl_zigbee_sec_man_key_t * | N/A | plaintext_key | [OUT] The key to export. |
Note
The context->derived_type must be SL_ZB_SEC_MAN_DERIVED_KEY_TYPE_NONE. Other values are ignored.
Returns
SL_STATUS_OK upon success, a valid error code otherwise.
sl_zigbee_sec_man_delete_transient_key#
sl_status_t sl_zigbee_sec_man_delete_transient_key (sl_zigbee_sec_man_context_t * context)
Search for a transient, or temporary, key and deletes it from key storage. Keys can be searched by EUI or key_index based on context->flags (see ::ZB_SEC_MAN_FLAG_EUI_IS_VALID and ::ZB_SEC_MAN_FLAG_KEY_INDEX_IS_VALID).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context | [IN] The context to use to look up a key entry. If the ZB_SEC_MAN_FLAG_EUI_IS_VALID flag is set in context->flags, then the context->eui field is used to search for and delete the key. If the ZB_SEC_MAN_FLAG_KEY_INDEX_IS_VALID flag is set in context->flags, then the context->key_index field is used to search for and delete the key. |
Returns
sl_status_t SL_STATUS_OK upon success, an error code otherwise.
sl_zigbee_sec_man_delete_key_table_key#
sl_status_t sl_zigbee_sec_man_delete_key_table_key (sl_zigbee_sec_man_context_t * context)
Delete the key table entry, or a key of type SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK, from storage. Keys can be searched by EUI or key_index based on context->flags (see ::ZB_SEC_MAN_FLAG_EUI_IS_VALID and ::ZB_SEC_MAN_FLAG_KEY_INDEX_IS_VALID).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context | [IN] The context to use to look up a key entry. If the ZB_SEC_MAN_FLAG_EUI_IS_VALID flag is set in context->flags, then the context->eui field is used to search for and delete the key. If the ZB_SEC_MAN_FLAG_KEY_INDEX_IS_VALID flag is set in context->flags, then the context->key_index field is used to search for and delete the key. |
Returns
sl_status_t SL_STATUS_OK upon success, an error code otherwise.
sl_zigbee_sec_man_check_key_context#
sl_status_t sl_zigbee_sec_man_check_key_context (sl_zigbee_sec_man_context_t * context)
Check that the passed key exists and can be successfully loaded. This function does not actually load the context, but only checks that it can be loaded.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context | [IN] The context to check for validity. The fields that must be set depend on the key type set in the context, as enough information is needed to identify the key. |
Returns
sl_status_t SL_STATUS_OK upon success, SL_STATUS_NOT_FOUND otherwise.
sl_zigbee_sec_man_get_network_key_info#
sl_status_t sl_zigbee_sec_man_get_network_key_info (sl_zigbee_sec_man_network_key_info_t * network_key_info)
Retrieve information about the network key and alternate network key. It will not retrieve the actual network key contents.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_network_key_info_t * | N/A | network_key_info | [OUT] The network key info struct used to store network key metadata, containing information about whether the current and next network keys are set, and the sequence numbers associated with each key. |
Returns
sl_status_t SL_STATUS_OK
sl_zigbee_sec_man_get_aps_key_info#
sl_status_t sl_zigbee_sec_man_get_aps_key_info (sl_zigbee_sec_man_context_t * context, sl_zigbee_sec_man_aps_key_metadata_t * key_data)
Retrieve metadata about an APS key. It does not retrieve the actual key contents.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context | [IN/OUT] The context to use to look up a key entry. If the user calls this function with the ::ZB_SEC_MAN_FLAG_KEY_INDEX_IS_VALID bit set in the context->flag field, then the key_index field in the context argument dictates which entry to retrieve. For keys with timeout and application link keys, the key_index retrieves the indexed entry into the respective table. Upon success, the eui64 field in the context is updated. If the user calls this function with the ::ZB_SEC_MAN_FLAG_EUI_IS_VALID bit set in the context->flag field, then the eui64 field in the context argument dictates which entry to retrieve. If the context->core_key_type argument is set to SL_ZB_SEC_MAN_KEY_TYPE_NETWORK, an error is returned as network keys are not tied to any specific EUI. If neither the ::ZB_SEC_MAN_FLAG_KEY_INDEX_IS_VALID bit nor the ::ZB_SEC_MAN_FLAG_EUI_IS_VALID bit is set in context->flags, then an error will be returned by this function. Upon success in fetching a key, the other fields in this argument are updated (e.g. a successful search by key_index will update the euii64 field). |
| sl_zigbee_sec_man_aps_key_metadata_t * | N/A | key_data | [OUT] Metadata to fill in. |
Returns
SL_STATUS_OK if successful, SL_STATUS_NOT_FOUND if the key_index or eui64 does not result in a found entry, SL_STATUS_INVALID_TYPE if the core key type is not an APS layer key (e.g. SL_ZB_SEC_MAN_KEY_TYPE_NETWORK), or SL_STATUS_INVALID_MODE if core_key_type is SL_ZB_SEC_MAN_KEY_TYPE_TC_LINK and the initial security state does not indicate the a preconfigured key has been set (that is, both SL_ZIGBEE_HAVE_PRECONFIGURED_KEY and SL_ZIGBEE_GET_PRECONFIGURED_KEY_FROM_INSTALL_CODE have not been set in the initial security state).
sl_zigbee_sec_man_delete_key#
sl_status_t sl_zigbee_sec_man_delete_key (sl_zigbee_sec_man_context_t * context)
Delete a key from storage. Certain keys are indexed, while others are not, as described here.
If context->core_key_type is..
..SL_ZB_SEC_MAN_KEY_TYPE_NETWORK, then context->key_index dictates whether to delete the current (active) network key (index 0) or the alternate network key (index 1).
..SL_ZB_SEC_MAN_KEY_TYPE_TC_LINK_WITH_TIMEOUT, then keys may be searched by context->eui64 or context->key_index. context->flags determines how to search (see ::sl_zigbee_sec_man_flags_t).
..SL_ZB_SEC_MAN_KEY_TYPE_APP_LINK, then keys may be searched by context->eui64 or context->key_index. context->flags determines how to search (see ::sl_zigbee_sec_man_flags_t).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context | [IN] The context to use to look up a key. |
..SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_PROXY_TABLE_KEY or SL_ZB_SEC_MAN_KEY_TYPE_GREEN_POWER_SINK_TABLE_KEY, then context->key_index dictates which key entry to delete. These Green Power keys are indexed keys, and there are SL_ZIGBEE_GP_PROXY_TABLE_SIZE/SL_ZIGBEE_GP_SINK_TABLE_SIZE many of them.
For all other key types, both context->key_index and context->eui64 are not used.
Returnssl_status_t SL_STATUS_OK upon success, an error code otherwise.
sl_zigbee_sec_man_load_key_context#
sl_status_t sl_zigbee_sec_man_load_key_context (sl_zigbee_sec_man_context_t * context)
Load the specified key into the Security Manager's internal context. Any subsequent crypto operations will be done with that loaded context.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context | [IN] The context to use to look up which key to load. If the derived key type is not SL_ZB_SEC_MAN_DERIVED_KEY_TYPE_NONE, then an appropriate key derivation scheme is applied to the key fetched according to the context supplied. |
Note
Enough information must be passed into context to properly identify the requested key, which is dependent on the key type requested. See sl_zigbee_sec_man_export_key for the requirements of the context argument based on core_key_type.
Returns
SL_STATUS_OK upon success, an error code otherwise.
sl_zigbee_sec_man_hmac_aes_mmo#
void sl_zigbee_sec_man_hmac_aes_mmo (const uint8_t * input, const uint8_t data_length, uint8_t * output)
Using a previously set key context, the Security Manager will perform an HMAC (keyed hash) using AES-MMO as the hashing algorithm, and AES-128 for the underlying block encryption.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | N/A | input | [IN] Data to be hashed. The keyed part of the keyed hash comes from the previously loaded context, so only data is input here. |
| const uint8_t | N/A | data_length | [IN] Length of the data to be hashed. |
| uint8_t * | N/A | output | [OUT] Hashed data. |
sl_zigbee_sec_man_aes_ccm_extended#
sl_status_t sl_zigbee_sec_man_aes_ccm_extended (uint8_t * nonce, bool encrypt, const uint8_t * input, uint8_t encryption_start_index, uint8_t length, uint8_t mic_length, uint8_t * output)
Encrypt/Decrypt the specified data using AES-CCM with AES-128 and a MIC of the requested length (in * bytes). See documentation for sl_zb_sec_ * man_aes_ccm for information on parameters besides mic_length.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | nonce | [IN] Nonce value used as part of CCM* encryption/decryption. |
| bool | N/A | encrypt | [IN] Encryption/decryption mode. True if encrypting, false for authenticated decryption. True when using this function for unauthenticated decryption (decrypt bytes in input and do not verify the end of input as a MIC). |
| const uint8_t * | N/A | input | [IN] Input to the CCM* encryption/decryption operation. The function assumes this is in packet format, where authenticated data begins at the location pointed to by input, and is followed by authenticated data. For authenticated decryption, the MIC is assumed to be located following the encrypted data. |
| uint8_t | N/A | encryption_start_index | [IN] Length of the authenticated data, equivalent to the index in input where data to be encrypted/decrypted begins. |
| uint8_t | N/A | length | [IN] Total length of authenticated + encrypted data excluding the MIC length. |
| uint8_t | N/A | mic_length | [IN] Length of the MIC to output. Currently supported MIC lengths are 4 bytes and 8 bytes. |
| uint8_t * | N/A | output |
sl_zigbee_sec_man_aes_ccm#
sl_status_t sl_zigbee_sec_man_aes_ccm (uint8_t * nonce, bool encrypt, const uint8_t * input, uint8_t encryption_start_index, uint8_t length, uint8_t * output)
Encrypt/Decrypt the specified data using AES-CCM with AES-128 and a 4-byte MIC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | nonce | [IN] Nonce value used as part of CCM* encryption. |
| bool | N/A | encrypt | [IN] Encryption/decryption mode. True if encrypting, false for authenticated decryption. True when using this function for unauthenticated decryption (decrypt bytes in input and do not verify the end of input as a MIC). |
| const uint8_t * | N/A | input | [IN] Input to the CCM* encryption operation. The function assumes this is in packet format, where authenticated data begins at the location pointed to by input, and is followed by authenticated data. For authenticated decryption, the MIC is assumed to be located following the encrypted data. |
| uint8_t | N/A | encryption_start_index | [IN] Length of the authenticated data, equivalent to the index in input where data to be encrypted/decrypted begins. |
| uint8_t | N/A | length | [IN] Total length of authenticated + encrypted data excluding the MIC length. |
| uint8_t * | N/A | output | [OUT] Output to the CCM* operation. When encrypt is true, this must have space for the input length plus a 4-byte MIC. For authenticated decryption, it must have size at least as large as the input length. |
sl_zigbee_sec_man_aes_128_crypt_block#
sl_status_t sl_zigbee_sec_man_aes_128_crypt_block (bool encrypt, const uint8_t * input, uint8_t * output)
Perform AES-128 crypto on the specified 16-byte block using a previously loaded context.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | encrypt | [IN] true if encrypting, else decrypt |
| const uint8_t * | N/A | input | [IN] Input, expected to be 16 bytes long. |
| uint8_t * | N/A | output | [OUT] Output of the AES-128 encryption operation. |
sl_zigbee_sec_man_find_symmetric_passphrase_key_table_index#
uint8_t sl_zigbee_sec_man_find_symmetric_passphrase_key_table_index (sl_802154_long_addr_t address)
Finds the Link Key Table index of the symmetric passphase of the given device EUI64.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_long_addr_t | N/A | address | EUI64 of device |
This function will return the Link Key Table index of the symmetric passphase of the given device EUI64, and will return 0xFF if no matching symmetric passphrase is found.
Returns
An uint8_t value that indicates the index of the stored symmetric passphrase in the link key table.
sl_zigbee_sec_man_import_symmetric_passphrase#
sl_status_t sl_zigbee_sec_man_import_symmetric_passphrase (uint8_t index, sl_802154_long_addr_t address, const sl_zigbee_key_data_t * key_data, key_data)
Imports the symmetric passphrase to the Link Key Table.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | whether to erase the key at the given index with matching address |
| sl_802154_long_addr_t | N/A | address | Link Key Table index to store symmetric passphrase |
| const sl_zigbee_key_data_t * | N/A | key_data | device EUI64 |
| N/A | key_data | pointer to symmetric passphrase memory |
This function will use Security Manager methods to store the given symmetric passphrase in the Link Key Table at the given index with matching EUI64.
Returns
An ::sl_status_t value that indicates the success or failure of importing the symmetric passphrase into the Link Key Table.
sl_zigbee_sec_man_export_symmetric_passphrase#
sl_status_t sl_zigbee_sec_man_export_symmetric_passphrase (sl_802154_long_addr_t address, sl_zigbee_key_data_t * key_data)
Exports the symmetric passphrase from the Link Key Table.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_long_addr_t | N/A | address | device EUI64 |
| sl_zigbee_key_data_t * | N/A | key_data | pointer to symmetric passphrase memory |
This function will use Security Manager methods to export the given symmetric passphrase from the Link Key Table matching EUI64.
Returns
An ::sl_status_t value that indicates the success or failure of exporting the symmetric passphrase into the Link Key Table.
sl_zigbee_sec_man_update_symmetric_passphrase_eui#
sl_status_t sl_zigbee_sec_man_update_symmetric_passphrase_eui (sl_802154_long_addr_t old_eui64, sl_802154_long_addr_t new_eui64)
Updates the device address of a symmetric passphrase entry.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_long_addr_t | N/A | old_eui64 | Old device address |
| sl_802154_long_addr_t | N/A | new_eui64 | New device address |
This function will update the device address of a symmetric passphrase entry in the Link Key Table that matches the given old device address with the new device address.
Returns
An ::sl_status_t value that indicates the success or failure of updating the Link Key Table entry's device EUI64
sl_zigbee_sec_man_link_key_slot_available#
bool sl_zigbee_sec_man_link_key_slot_available (sl_802154_long_addr_t eui64)
Checks whether a new link key with a device can be stored.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_long_addr_t | N/A | eui64 | device address |
Returns
True if a new link key could be stored (there is either an existing entry with this device's EUI64 or a free entry for a new device), false if not (table is full).
sl_zigbee_sec_man_compare_key_to_value#
bool sl_zigbee_sec_man_compare_key_to_value (sl_zigbee_sec_man_context_t * context, const sl_zigbee_sec_man_key_t * test_key)
Check whether the key referenced by a given context has a specified value. This API is only compatible with keys that permit the standard Zigbee encryption algorithm and have a core key type that is not SL_ZB_SEC_MAN_KEY_TYPE_INTERNAL.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_sec_man_context_t * | N/A | context | Reference to the key being checked |
| const sl_zigbee_sec_man_key_t * | N/A | test_key | Value to test for |
Returns
True if the key referenced by context has the value test_key, false otherwise.