Find and Bind Initiator#
Callbacks for Find and Bind Initiator Component.
Callbacks#
Callback fired when a potential bind target has been found.
Find and Bind Complete.
Callbacks Documentation#
sl_zigbee_af_find_and_bind_initiator_bind_target_cb#
bool sl_zigbee_af_find_and_bind_initiator_bind_target_cb (sl_802154_short_addr_t nodeId, sl_zigbee_binding_table_entry_t * bindingEntry, uint8_t * groupName)
Callback fired when a potential bind target has been found.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_802154_short_addr_t | [out] | nodeId | short ID of the potential target Ver.: always |
| sl_zigbee_binding_table_entry_t * | [out] | bindingEntry | The binding entry for that target. Ver.: always |
| uint8_t * | [out] | groupName | The name of the group if a multicast binding is created. Ver.: always |
This callback with enable the user to programmatically decide if they want to bind with a potential target. The plugin will try to bind with this target if and only if the function returns true. By default, the callback tells the plugin to try to bind with the target. If the binding type is changed to ::SL_ZIGBEE_MULTICAST_BINDING, a multicast binding will be created.
Returns
Whether or not to bind to target. Defaults to true.
sl_zigbee_af_find_and_bind_initiator_complete_cb#
void sl_zigbee_af_find_and_bind_initiator_complete_cb (sl_status_t status)
Find and Bind Complete.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_status_t | [out] | status | Status code describing the completion of the find and bind process Ver.: always |
This callback is fired by the initiator when the Find and Bind process is complete.