Level Control#

Callbacks for Level Control Component.

Callbacks#

void

Level control cluster server post init.

void

Level control coupled color temp change.

Callbacks Documentation#

sl_zigbee_af_level_control_cluster_server_post_init_cb#

void sl_zigbee_af_level_control_cluster_server_post_init_cb (uint8_t endpoint)

Level control cluster server post init.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint

Endpoint that is being initialized Ver.: always

Following the resolution of the current level at startup for this endpoint, perform any additional initialization needed, e.g., synchronize hardware state.


sl_zigbee_af_level_control_coupled_color_temp_change_cb#

void sl_zigbee_af_level_control_coupled_color_temp_change_cb (uint8_t endpoint)

Level control coupled color temp change.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint

Endpoint that is being initialized Ver.: always

Adjust color control cluster color temperature in response to a change in level control cluster CurrentLevel.