OTA Storage#
Callbacks for OTA Storage Component.
Callbacks#
sl_zigbee_af_ota_storage_delete_image_cb(const sl_zigbee_af_ota_image_id_t *id)
A callback returning the status of the OTA storage deleting an image.
uint32_t
OTA Storage Driver max download size callback.
Callbacks Documentation#
sl_zigbee_af_ota_storage_delete_image_cb#
sl_zigbee_af_ota_storage_status_t sl_zigbee_af_ota_storage_delete_image_cb (const sl_zigbee_af_ota_image_id_t * id)
A callback returning the status of the OTA storage deleting an image.
Parameters
Type | Direction | Argument Name | Description |
---|---|---|---|
const sl_zigbee_af_ota_image_id_t * | [in] | id | a pointer of type: sl_zigbee_af_ota_image_id_t referring to the OTA image ID |
Returns
A sl_zigbee_af_ota_storage_status_t on if image deletion was successful.
sl_zigbee_af_ota_storage_driver_max_download_size_cb#
uint32_t sl_zigbee_af_ota_storage_driver_max_download_size_cb (void )
OTA Storage Driver max download size callback.
Parameters
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
A ::uint32_t on the maximum download size for the OTA file.