Prepayment Server#

Callbacks for Prepayment Server Component.

Callbacks#

void
sl_zigbee_af_prepayment_cluster_server_attribute_changed_cb(uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId)

Prepayment Cluster Server Attribute Changed.

void
sl_zigbee_af_prepayment_cluster_server_default_response_cb(uint8_t endpoint, uint8_t commandId, sl_zigbee_af_status_t status)

Prepayment cluster server default response.

void

Initialize the prepayment cluster server.

void
sl_zigbee_af_prepayment_cluster_server_manufacturer_specific_attribute_changed_cb(uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, uint16_t manufacturerCode)

Prepayment cluster server manufacturer-specific attribute changed.

void
sl_zigbee_af_prepayment_cluster_server_message_sent_cb(sl_zigbee_outgoing_message_type_t type, uint16_t indexOrDestination, sl_zigbee_aps_frame_t *apsFrame, uint16_t msgLen, uint8_t *message, sl_status_t status)

Prepayment cluster server message sent.

sl_zigbee_af_prepayment_cluster_server_pre_attribute_changed_cb(uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, sl_zigbee_af_attribute_type_t attributeType, uint8_t size, uint8_t *value)

Prepayment cluster server pre attribute changed.

Callbacks Documentation#

sl_zigbee_af_prepayment_cluster_server_attribute_changed_cb#

void sl_zigbee_af_prepayment_cluster_server_attribute_changed_cb (uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId)

Prepayment Cluster Server Attribute Changed.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint

Endpoint that is being initialized Ver.: always

sl_zigbee_af_attribute_id_tN/AattributeId

Attribute that changed Ver.: always


sl_zigbee_af_prepayment_cluster_server_default_response_cb#

void sl_zigbee_af_prepayment_cluster_server_default_response_cb (uint8_t endpoint, uint8_t commandId, sl_zigbee_af_status_t status)

Prepayment cluster server default response.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint

Destination endpoint Ver.: always

uint8_tN/AcommandId

Command id Ver.: always

sl_zigbee_af_status_tN/Astatus

Status in default response Ver.: always

This function is called when the server receives the default response from the client.


sl_zigbee_af_prepayment_cluster_server_init_cb#

void sl_zigbee_af_prepayment_cluster_server_init_cb (uint8_t endpoint)

Initialize the prepayment cluster server.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint

Endpoint that is being initialized Ver.: always


sl_zigbee_af_prepayment_cluster_server_manufacturer_specific_attribute_changed_cb#

void sl_zigbee_af_prepayment_cluster_server_manufacturer_specific_attribute_changed_cb (uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, uint16_t manufacturerCode)

Prepayment cluster server manufacturer-specific attribute changed.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint

Endpoint that is being initialized Ver.: always

sl_zigbee_af_attribute_id_tN/AattributeId

Attribute that changed Ver.: always

uint16_tN/AmanufacturerCode

Manufacturer Code of the attribute that changed Ver.: always


sl_zigbee_af_prepayment_cluster_server_message_sent_cb#

void sl_zigbee_af_prepayment_cluster_server_message_sent_cb (sl_zigbee_outgoing_message_type_t type, uint16_t indexOrDestination, sl_zigbee_aps_frame_t * apsFrame, uint16_t msgLen, uint8_t * message, sl_status_t status)

Prepayment cluster server message sent.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_outgoing_message_type_tN/Atype

The type of message sent Ver.: always

uint16_tN/AindexOrDestination

The destination or address to which the message was sent Ver.: always

sl_zigbee_aps_frame_t *N/AapsFrame

The APS frame for the message Ver.: always

uint16_tN/AmsgLen

The length of the message Ver.: always

uint8_t *N/Amessage

The message that was sent Ver.: always

sl_status_tN/Astatus

The status of the sent message Ver.: always


sl_zigbee_af_prepayment_cluster_server_pre_attribute_changed_cb#

sl_zigbee_af_status_t sl_zigbee_af_prepayment_cluster_server_pre_attribute_changed_cb (uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, sl_zigbee_af_attribute_type_t attributeType, uint8_t size, uint8_t * value)

Prepayment cluster server pre attribute changed.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint

Endpoint that is being initialized Ver.: always

sl_zigbee_af_attribute_id_tN/AattributeId

Attribute to be changed Ver.: always

sl_zigbee_af_attribute_type_tN/AattributeType

Attribute type Ver.: always

uint8_tN/Asize

Attribute size Ver.: always

uint8_t *N/Avalue

Attribute value Ver.: always