Sleepy Message Queue#
Callbacks for Sleepy Message Queue Component.
Callbacks#
void
sl_zigbee_af_sleepy_message_queue_init_cb(uint8_t init_level)
Initialize the sleepy message queue.
void
sl_zigbee_af_sleepy_message_queue_message_timed_out_cb(uint8_t sleepyMsgId)
Message time out.
Callbacks Documentation#
sl_zigbee_af_sleepy_message_queue_init_cb#
void sl_zigbee_af_sleepy_message_queue_init_cb (uint8_t init_level)
Initialize the sleepy message queue.
Parameters
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | init_level | Initialize event and local data
|
sl_zigbee_af_sleepy_message_queue_message_timed_out_cb#
void sl_zigbee_af_sleepy_message_queue_message_timed_out_cb (uint8_t sleepyMsgId)
Message time out.
Parameters
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | sleepyMsgId | Ver.: always |
This function is called by the sleepy message queue when a message times out. The plugin will invalidate the entry in the queue after giving the application a chance to perform any actions on the timed-out message.