Data point descriptor. Compact attribute, Multi sensor or Generic switch feature uses this as descriptor to interpret the incoming data from the GPD. This descriptor is set up at the sink during the commissioning.

Public Attribute Documentation#

nbAttrRecord#

uint8_t sl_zigbee_gp_data_point_descriptor_t::nbAttrRecord

Number of attribute records


Definition at line 651 of file stack/include/gp-types.h

clientServer#

uint8_t sl_zigbee_gp_data_point_descriptor_t::clientServer

Client or Server flag


Definition at line 653 of file stack/include/gp-types.h

ManIdPresent#

uint8_t sl_zigbee_gp_data_point_descriptor_t::ManIdPresent

Manufacture ID present


Definition at line 655 of file stack/include/gp-types.h

datapointOptions#

uint8_t sl_zigbee_gp_data_point_descriptor_t::datapointOptions

Data point options


Definition at line 657 of file stack/include/gp-types.h

clusterID#

uint16_t sl_zigbee_gp_data_point_descriptor_t::clusterID

Cluster ID


Definition at line 659 of file stack/include/gp-types.h

manufacturerID#

uint16_t sl_zigbee_gp_data_point_descriptor_t::manufacturerID

Manufacture ID


Definition at line 661 of file stack/include/gp-types.h

attrRecord#

sl_zigbee_gp_attribute_record_t sl_zigbee_gp_data_point_descriptor_t::attrRecord

Attribute Record


Definition at line 663 of file stack/include/gp-types.h