Generic Switch Information. Generic switch feature uses this as descriptor to interpret the incoming switch command from the GPD. This information is set up at the sink during the commissioning.
Public Attribute Documentation#
switchInfoLength#
uint8_t sl_zigbee_gp_switch_information_t::switchInfoLength
Switch Information Length
Definition at line
690
of file stack/include/gp-types.h
nbOfContacts#
uint8_t sl_zigbee_gp_switch_information_t::nbOfContacts
Number of contacts in the switch
Definition at line
692
of file stack/include/gp-types.h
switchType#
uint8_t sl_zigbee_gp_switch_information_t::switchType
Switch type
Definition at line
694
of file stack/include/gp-types.h
currentContact#
uint8_t sl_zigbee_gp_switch_information_t::currentContact
Current contact
Definition at line
696
of file stack/include/gp-types.h
savedContact#
uint8_t sl_zigbee_gp_switch_information_t::savedContact
Saved contacts
Definition at line
698
of file stack/include/gp-types.h