Additional Information Block Option Record Fields. Provides information regarding the record fields from the linked translation table. Typically, a translation table, which contains the generic switch, multi sensor or the compact attribute reporting GPD, needs to populate the information during commissioning and use it to translate the shorter GPDF to the longer ZCL payload.

Public Attributes#

uint16_t
uint16_t
struct sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9::@10
struct sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9::@11
union sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9

Public Attribute Documentation#

totalLengthOfAddInfoBlock#

uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::totalLengthOfAddInfoBlock

Total Length of the additional information block


Definition at line 721 of file stack/include/gp-types.h

optionSelector#

uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::optionSelector

Option selector


Definition at line 723 of file stack/include/gp-types.h

reportIdentifier#

uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::reportIdentifier

Definition at line 727 of file stack/include/gp-types.h

attrOffsetWithinReport#

uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::attrOffsetWithinReport

Definition at line 728 of file stack/include/gp-types.h

clusterID#

uint16_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::clusterID

Definition at line 729 of file stack/include/gp-types.h

attributeID#

uint16_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::attributeID

Definition at line 730 of file stack/include/gp-types.h

attributeDataType#

uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::attributeDataType

Definition at line 731 of file stack/include/gp-types.h

attributeOptions#

uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::attributeOptions

Definition at line 732 of file stack/include/gp-types.h

manufacturerID#

uint16_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::manufacturerID

Definition at line 733 of file stack/include/gp-types.h

compactAttr#

struct sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9::@10 sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::compactAttr

Compact Attribute Reporting or Multi sensor


Definition at line 734 of file stack/include/gp-types.h

contactStatus#

uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::contactStatus

Provides button information of the Generic switch for contacts status


Definition at line 738 of file stack/include/gp-types.h

contactBitmask#

uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::contactBitmask

Provides the bitmask to evaluate the received contact. As a result, the bitmask only depends on the number of contacts of the current GPD.


Definition at line 742 of file stack/include/gp-types.h

genericSwitch#

struct sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9::@11 sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::genericSwitch

Generic switch information


Definition at line 743 of file stack/include/gp-types.h

optionData#

union sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9 sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::optionData

Definition at line 744 of file stack/include/gp-types.h