Report descriptor. Compact attribute or Multi sensor feature uses this as descriptor to interpret the incoming report from the GPD. This descriptor is set up at the sink during the commissioning.

Public Attribute Documentation#

repId#

uint8_t sl_zigbee_gp_report_descriptor_t::repId

Report ID


Definition at line 673 of file stack/include/gp-types.h

reportOptions#

uint8_t sl_zigbee_gp_report_descriptor_t::reportOptions

Report options


Definition at line 675 of file stack/include/gp-types.h

timeoutPeriod#

uint16_t sl_zigbee_gp_report_descriptor_t::timeoutPeriod

Report timeout period


Definition at line 677 of file stack/include/gp-types.h

totalLength#

uint8_t sl_zigbee_gp_report_descriptor_t::totalLength

Total length of report


Definition at line 679 of file stack/include/gp-types.h

dataPoint#

sl_zigbee_gp_data_point_descriptor_t sl_zigbee_gp_report_descriptor_t::dataPoint

Report data point descriptor


Definition at line 681 of file stack/include/gp-types.h