sl_bt_evt_cs_config_complete#

Indicates that a locally initiated ABR configuration procedure has completed or the local controller has responded to an ABR configuration request from the remote controller.

Modules#

sl_bt_evt_cs_config_complete_s

Macros#

#define

Identifier of the config_complete event.

Typedef Documentation#

sl_bt_evt_cs_config_complete_t#

typedef struct sl_bt_evt_cs_config_complete_s sl_bt_evt_cs_config_complete_t

Definition at line 12609 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_cs_config_complete_id#

#define sl_bt_evt_cs_config_complete_id
Value:
0x015900a0

Identifier of the config_complete event.


Definition at line 12408 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h