sl_bt_evt_dfu_boot#
This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).
Modules#
sl_bt_evt_dfu_boot_s
Macros#
#define
Identifier of the boot event.
Typedef Documentation#
sl_bt_evt_dfu_boot_t#
typedef struct sl_bt_evt_dfu_boot_s sl_bt_evt_dfu_boot_t
Definition at line 142
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_dfu_boot_id#
#define sl_bt_evt_dfu_boot_id
Value:0x000000a0
Identifier of the boot event.
Definition at line 132
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h