sl_bt_evt_gatt_descriptor_value#

Indicates that the value of a descriptor in the remote GATT server was received.

This event is generated by the sl_bt_gatt_read_descriptor_value command.

Modules#

sl_bt_evt_gatt_descriptor_value_s

Macros#

#define

Identifier of the descriptor_value event.

Typedef Documentation#

sl_bt_evt_gatt_descriptor_value_t#

typedef struct sl_bt_evt_gatt_descriptor_value_s sl_bt_evt_gatt_descriptor_value_t

Definition at line 7980 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_gatt_descriptor_value_id#

#define sl_bt_evt_gatt_descriptor_value_id
Value:
0x050900a0

Identifier of the descriptor_value event.


Definition at line 7967 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h