Data structure of the response_report event.

Public Attributes#

uint8_t
int8_t
int8_t
uint8_t
uint8_t

Public Attribute Documentation#

advertising_set#

uint8_t sl_bt_evt_pawr_advertiser_response_report_s::advertising_set

The PAwR advertising set handle


Definition at line 6097 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

subevent#

uint8_t sl_bt_evt_pawr_advertiser_response_report_s::subevent

The subevent that this report corresponds to


Definition at line 6098 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

tx_power#

int8_t sl_bt_evt_pawr_advertiser_response_report_s::tx_power

TX power value in the received packet header. Units: dBm

  • Valid value range: -127 to 126

  • Value 127: information unavailable


Definition at line 6099 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

rssi#

int8_t sl_bt_evt_pawr_advertiser_response_report_s::rssi

Signal strength indicator (RSSI) of the received packet. Units: dBm

  • Valid value range: -127 to +20

  • Value 127: information unavailable


Definition at line 6103 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

cte_type#

uint8_t sl_bt_evt_pawr_advertiser_response_report_s::cte_type

The CTE type

  • 0x00: AoA CTE

  • 0x01: AoD CTE with 1us slots

  • 0x02: AoD CTE with 2us slots

  • 0xFF: No CTE


Definition at line 6107 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

response_slot#

uint8_t sl_bt_evt_pawr_advertiser_response_report_s::response_slot

The response slot that this report corresponds to


Definition at line 6112 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

data_status#

uint8_t sl_bt_evt_pawr_advertiser_response_report_s::data_status

Data completeness:

  • 0: Complete

  • 1: Incomplete, more data to come in new events

  • 2: Incomplete, data truncated, no more to come

  • 255: Failed to receive subevent response in this response slot


Definition at line 6114 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

counter#

uint8_t sl_bt_evt_pawr_advertiser_response_report_s::counter

The sequence number of this sl_bt_evt_pawr_advertiser_response_report event as a monotonically increasing counter that wraps from 255 to 0. There is a single counter for this event type that starts from value 0 when the Bluetooth stack is started and is never reset while the stack is running. This counter can be used to detect if one or more sl_bt_evt_pawr_advertiser_response_report events have been created by the stack but dropped due to problems such as temporarily running out of resources before the event reached the application.


Definition at line 6122 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

data#

uint8array sl_bt_evt_pawr_advertiser_response_report_s::data

The response data that was received, if any


Definition at line 6136 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h