sl_bt_evt_scanner_extended_advertisement_report#
Reports an advertising or scan response packet from an advertising device that uses extended advertising PDUs.
Multiple events may be reported for single advertisement train.
This event is used to report advertisements only if the application includes the bluetooth_feature_extended_scanner component. Otherwise, the sl_bt_evt_scanner_scan_report event is used for maintaining the backwards compatibility.
Modules#
sl_bt_evt_scanner_extended_advertisement_report_s
Typedefs#
Macros#
#define
Identifier of the extended_advertisement_report event.
Typedef Documentation#
sl_bt_evt_scanner_extended_advertisement_report_t#
typedef struct sl_bt_evt_scanner_extended_advertisement_report_s sl_bt_evt_scanner_extended_advertisement_report_t
Definition at line
4090
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_scanner_extended_advertisement_report_id#
#define sl_bt_evt_scanner_extended_advertisement_report_idValue:
0x020500a0
Identifier of the extended_advertisement_report event.
Definition at line
3938
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h