sl_bt_evt_sm_passkey_request#

Indicates a request for the passkey prompt displayed on the remote device.

Use the command sl_bt_sm_enter_passkey to input the passkey value.

Modules#

sl_bt_evt_sm_passkey_request_s

Macros#

#define

Identifier of the passkey_request event.

Typedef Documentation#

sl_bt_evt_sm_passkey_request_t#

typedef struct sl_bt_evt_sm_passkey_request_s sl_bt_evt_sm_passkey_request_t

Definition at line 10641 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_sm_passkey_request_id#

#define sl_bt_evt_sm_passkey_request_id
Value:
0x010f00a0

Identifier of the passkey_request event.


Definition at line 10631 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h