sl_bt_evt_sync_transfer_received#

Deprecated and replaced by sl_bt_evt_periodic_sync_transfer_received for periodic advertising trains that do not have subevents or response slots responses, and with sl_bt_evt_pawr_sync_transfer_received for Periodic Advertising with Responses (PAwR) trains.

Indicates that synchronization information for a periodic advertising train has been received

See PAST Receiver.

Modules#

sl_bt_evt_sync_transfer_received_s

Macros#

#define

Identifier of the transfer_received event.

Typedef Documentation#

sl_bt_evt_sync_transfer_received_t#

typedef struct sl_bt_evt_sync_transfer_received_s sl_bt_evt_sync_transfer_received_t

Definition at line 4781 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_sync_transfer_received_id#

#define sl_bt_evt_sync_transfer_received_id
Value:
0x034200a0

Identifier of the transfer_received event.


Definition at line 4716 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h