sl_bt_evt_system_hardware_error#
Indicates that a hardware-related error has occurred.
Modules#
sl_bt_evt_system_hardware_error_s
Typedefs#
Macros#
#define
sl_bt_evt_system_hardware_error_id 0x050100a0
Identifier of the hardware_error event.
Typedef Documentation#
sl_bt_evt_system_hardware_error_t#
typedef struct sl_bt_evt_system_hardware_error_s sl_bt_evt_system_hardware_error_t
Definition at line
842
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_system_hardware_error_id#
#define sl_bt_evt_system_hardware_error_idValue:
0x050100a0
Identifier of the hardware_error event.
Definition at line
832
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h