Transmit Power Reporting Constants#

Constants in transmit power reporting

Macro Definition Documentation#

SL_BT_CONNECTION_TX_POWER_UNMANAGED#

#define SL_BT_CONNECTION_TX_POWER_UNMANAGED
Value:
0x7e

Remote device is not managing power levels.


Definition at line 6486 of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

SL_BT_CONNECTION_TX_POWER_UNAVAILABLE#

#define SL_BT_CONNECTION_TX_POWER_UNAVAILABLE
Value:
0x7f

Transmit power level is not available.


Definition at line 6489 of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

SL_BT_CONNECTION_TX_POWER_CHANGE_UNAVAILABLE#

#define SL_BT_CONNECTION_TX_POWER_CHANGE_UNAVAILABLE
Value:
0x7f

Change is not available or is out of range.


Definition at line 6492 of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h