sl_bt_evt_connection_statistics#
Provides the connection statistic values when the application includes the component bluetooth_feature_connection_statistics.
When the component is included by the application, this event is automatically triggered to provide the final statistics for the connection just before the sl_bt_evt_connection_closed event indicates that a connection has been closed. This event is also triggered when the application has requested reading the statistics using the command sl_bt_connection_read_statistics.
Modules#
sl_bt_evt_connection_statistics_s
Typedefs#
Macros#
#define
sl_bt_evt_connection_statistics_id 0x0a0600a0
Identifier of the statistics event.
Typedef Documentation#
sl_bt_evt_connection_statistics_t#
typedef struct sl_bt_evt_connection_statistics_s sl_bt_evt_connection_statistics_t
Definition at line
7001
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_connection_statistics_id#
#define sl_bt_evt_connection_statistics_idValue:
0x0a0600a0
Identifier of the statistics event.
Definition at line
6939
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h