sl_bt_evt_connection_set_parameters_failed#
Triggered when the peer device rejected an L2CAP connection parameter update request as a result of calling command sl_bt_connection_set_parameters to change connection parameters on the sl_bt_connection_role_peripheral role.
Modules#
sl_bt_evt_connection_set_parameters_failed_s
Typedefs#
Macros#
#define
Identifier of the set_parameters_failed event.
Typedef Documentation#
sl_bt_evt_connection_set_parameters_failed_t#
typedef struct sl_bt_evt_connection_set_parameters_failed_s sl_bt_evt_connection_set_parameters_failed_t
Definition at line
6638
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_connection_set_parameters_failed_id#
#define sl_bt_evt_connection_set_parameters_failed_idValue:
0x100600a0
Identifier of the set_parameters_failed event.
Definition at line
6628
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h