sl_bt_evt_connection_parameters#
Triggered whenever the connection parameters are changed and at any time a connection is established.
Modules#
sl_bt_evt_connection_parameters_s
Typedefs#
Macros#
#define
sl_bt_evt_connection_parameters_id 0x020600a0
Identifier of the parameters event.
Typedef Documentation#
sl_bt_evt_connection_parameters_t#
typedef struct sl_bt_evt_connection_parameters_s sl_bt_evt_connection_parameters_t
Definition at line
6614
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_connection_parameters_id#
#define sl_bt_evt_connection_parameters_idValue:
0x020600a0
Identifier of the parameters event.
Definition at line
6584
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h