sl_bt_evt_connection_closed#
Indicates that a connection was either closed or that no connection was established from a high duty cycle directed advertising.
If the application includes the component bluetooth_feature_connection_statistics and the connection was successfully opened, the event sl_bt_evt_connection_statistics is automatically triggered just before the connection closed event to provide the application with the final statistic values of the connection.
Modules#
Typedefs#
typedef struct sl_bt_evt_connection_closed_s
Macros#
#define
sl_bt_evt_connection_closed_id 0x010600a0
Identifier of the closed event.