You are viewing documentation for version:
Data structure of the rssi event. 
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_connection_rssi_s::connection
Connection handle 
status#
uint8_t sl_bt_evt_connection_rssi_s::status
Command complete status which is always SL_STATUS_OK 
rssi
int8_t sl_bt_evt_connection_rssi_s::rssi
The median of the last seven measured RSSI values on the connection. Units: dBm. Range: -127 to +20.