sl_bt_evt_cs_config_complete#
Indicates that a locally initiated ABR configuration procedure has completed or the local controller has responded to an ABR configuration request from the remote controller.
Modules#
sl_bt_evt_cs_config_complete_s
Typedefs#
typedef struct sl_bt_evt_cs_config_complete_s
Macros#
#define
sl_bt_evt_cs_config_complete_id 0x015900a0
Identifier of the config_complete event.
Typedef Documentation#
sl_bt_evt_cs_config_complete_t#
typedef struct sl_bt_evt_cs_config_complete_s sl_bt_evt_cs_config_complete_t
Definition at line
12855
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_cs_config_complete_id#
#define sl_bt_evt_cs_config_complete_idValue:
0x015900a0
Identifier of the config_complete event.
Definition at line
12633
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h