sl_bt_evt_cs_procedure_enable_complete#
Indicates the controller has scheduled a new ABR procedure measurement, as a result of sl_bt_cs_procedure_enable command or disabled an ongoing, as a result of sl_bt_cs_procedure_enable command.
Modules#
sl_bt_evt_cs_procedure_enable_complete_s
Typedefs#
Macros#
#define
sl_bt_evt_cs_procedure_enable_complete_id 0x025900a0
Identifier of the procedure_enable_complete event.
Typedef Documentation#
sl_bt_evt_cs_procedure_enable_complete_t#
typedef struct sl_bt_evt_cs_procedure_enable_complete_s sl_bt_evt_cs_procedure_enable_complete_t
Definition at line
12916
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_cs_procedure_enable_complete_id#
#define sl_bt_evt_cs_procedure_enable_complete_idValue:
0x025900a0
Identifier of the procedure_enable_complete event.
Definition at line
12868
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h