Data structure of the characteristic event.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_gatt_characteristic_s::connection

Connection handle


Definition at line 8063 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

characteristic#

uint16_t sl_bt_evt_gatt_characteristic_s::characteristic

GATT characteristic handle


Definition at line 8064 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

properties#

uint8_t sl_bt_evt_gatt_characteristic_s::properties

Characteristic properties


Definition at line 8065 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

uuid#

uint8array sl_bt_evt_gatt_characteristic_s::uuid

Characteristic UUID in little endian format


Definition at line 8066 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h