sl_bt_evt_gatt_server_indication_timeout#

Indicates confirmation from the remote GATT client has not been received within 30 seconds after an indication was sent.

Furthermore, the stack does not allow GATT transactions over this connection.

Modules#

sl_bt_evt_gatt_server_indication_timeout_s

Macros#

#define

Identifier of the indication_timeout event.

Typedef Documentation#

sl_bt_evt_gatt_server_indication_timeout_t#

typedef struct sl_bt_evt_gatt_server_indication_timeout_s sl_bt_evt_gatt_server_indication_timeout_t

Definition at line 9769 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_gatt_server_indication_timeout_id#

#define sl_bt_evt_gatt_server_indication_timeout_id
Value:
0x050a00a0

Identifier of the indication_timeout event.


Definition at line 9759 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h