sl_bt_evt_gatt_server_attribute_value#
Indicates that the value of an attribute in the local GATT database was changed by a remote GATT client.
The parameter att_opcode
describes which GATT procedure was used to change the value.
Modules#
sl_bt_evt_gatt_server_attribute_value_s
Typedefs#
Macros#
#define
sl_bt_evt_gatt_server_attribute_value_id 0x000a00a0
Identifier of the attribute_value event.
Typedef Documentation#
sl_bt_evt_gatt_server_attribute_value_t#
typedef struct sl_bt_evt_gatt_server_attribute_value_s sl_bt_evt_gatt_server_attribute_value_t
Definition at line
9588
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_gatt_server_attribute_value_id#
#define sl_bt_evt_gatt_server_attribute_value_idValue:
0x000a00a0
Identifier of the attribute_value event.
Definition at line
9572
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h