sl_bt_evt_test_dtm_completed#
Indicates that the radio has processed a test start or end command.
The result
parameter indicates the success of the command.
After the receiver or transmitter test is stopped, the number_of_packets
parameter in this event indicates the number of received or transmitted packets.
Modules#
sl_bt_evt_test_dtm_completed_s
Typedefs#
typedef struct sl_bt_evt_test_dtm_completed_s
Macros#
#define
sl_bt_evt_test_dtm_completed_id 0x000e00a0
Identifier of the dtm_completed event.
Typedef Documentation#
sl_bt_evt_test_dtm_completed_t#
typedef struct sl_bt_evt_test_dtm_completed_s sl_bt_evt_test_dtm_completed_t
Definition at line
10412
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_test_dtm_completed_id#
#define sl_bt_evt_test_dtm_completed_idValue:
0x000e00a0
Identifier of the dtm_completed event.
Definition at line
10398
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h