You are viewing documentation for version:
sl_bt_evt_connection_rssi
Triggered when a sl_bt_connection_get_rssi command has completed.
This event is only used by deprecated sl_bt_connection_get_rssi that returns the RSSI value asynchronously.
Use the sl_bt_connection_get_median_rssi command to get the RSSI synchronously.
Modules#
sl_bt_evt_connection_rssi_s
Macros#
#define
Identifier of the rssi event.
Typedef Documentation#
sl_bt_evt_connection_rssi_t
typedef struct sl_bt_evt_connection_rssi_s sl_bt_evt_connection_rssi_t
Definition at line 6072
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_connection_rssi_id
#define sl_bt_evt_connection_rssi_id
Value:0x030600a0
Identifier of the rssi event.
Definition at line 6059
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h