sl_bt_evt_connection_data_length#
Reports a change to the maximum payload length or maximum TX time in either direction of a connection.
Modules#
sl_bt_evt_connection_data_length_s
Macros#
#define
Identifier of the data_length event.
Typedef Documentation#
sl_bt_evt_connection_data_length_t#
typedef struct sl_bt_evt_connection_data_length_s sl_bt_evt_connection_data_length_t
Definition at line 5926
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_connection_data_length_id#
#define sl_bt_evt_connection_data_length_id
Value:0x090600a0
Identifier of the data_length event.
Definition at line 5908
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h