Data structure of the data_length event.

Public Attributes#

uint8_t
uint16_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_connection_data_length_s::connection

Connection handle


tx_data_len#

uint16_t sl_bt_evt_connection_data_length_s::tx_data_len

The maximum payload octets of a packet that the local Controller will send


tx_time_us#

uint16_t sl_bt_evt_connection_data_length_s::tx_time_us

The maximum time in microseconds that the local Controller will take to send a data packet


rx_data_len#

uint16_t sl_bt_evt_connection_data_length_s::rx_data_len

The maximum payload octets of a packet that the local Controller expects to receive


rx_time_us#

uint16_t sl_bt_evt_connection_data_length_s::rx_time_us

The maximum time in microseconds that the local Controller expects to take to receive a data packet