You are viewing documentation for version:
sl_bt_evt_external_bondingdb_data#
Indicates that updated bonding data of a connection is available.
The application must store it in the external bonding database permanently.
Modules#
sl_bt_evt_external_bondingdb_data_s
Macros#
#define
Identifier of the data event.
Typedef Documentation#
sl_bt_evt_external_bondingdb_data_t#
typedef struct sl_bt_evt_external_bondingdb_data_s sl_bt_evt_external_bondingdb_data_t
Definition at line 10846
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_external_bondingdb_data_id#
#define sl_bt_evt_external_bondingdb_data_id
Value:0x015c00a0
Identifier of the data event.
Definition at line 10793
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h