sl_bt_evt_external_bondingdb_data_ready#
Indicates that stack has received all the necessary bonding data from the application and is now fully functional.
Modules#
sl_bt_evt_external_bondingdb_data_ready_s
Typedefs#
Macros#
#define
sl_bt_evt_external_bondingdb_data_ready_id 0x025c00a0
Identifier of the data_ready event.
Typedef Documentation#
sl_bt_evt_external_bondingdb_data_ready_t#
typedef struct sl_bt_evt_external_bondingdb_data_ready_s sl_bt_evt_external_bondingdb_data_ready_t
Definition at line
10868
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_external_bondingdb_data_ready_id#
#define sl_bt_evt_external_bondingdb_data_ready_idValue:
0x025c00a0
Identifier of the data_ready event.
Definition at line
10858
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h