sl_bt_evt_gatt_server_indication_timeout#
Indicates confirmation from the remote GATT client has not been received within 30 seconds after an indication was sent.
Furthermore, the stack does not allow GATT transactions over this connection.
Modules#
sl_bt_evt_gatt_server_indication_timeout_s
Typedefs#
Macros#
#define
sl_bt_evt_gatt_server_indication_timeout_id 0x050a00a0
Identifier of the indication_timeout event.
Typedef Documentation#
sl_bt_evt_gatt_server_indication_timeout_t#
typedef struct sl_bt_evt_gatt_server_indication_timeout_s sl_bt_evt_gatt_server_indication_timeout_t
Definition at line
8843
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_gatt_server_indication_timeout_id#
#define sl_bt_evt_gatt_server_indication_timeout_idValue:
0x050a00a0
Identifier of the indication_timeout event.
Definition at line
8833
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h