sl_bt_evt_gatt_server_execute_write_completed#
Indicates that the execute write command from a remote GATT client has completed with the given result.
Modules#
sl_bt_evt_gatt_server_execute_write_completed_s
Typedefs#
Macros#
#define
Identifier of the execute_write_completed event.
Typedef Documentation#
sl_bt_evt_gatt_server_execute_write_completed_t#
typedef struct sl_bt_evt_gatt_server_execute_write_completed_s sl_bt_evt_gatt_server_execute_write_completed_t
Definition at line
8819
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_gatt_server_execute_write_completed_id#
#define sl_bt_evt_gatt_server_execute_write_completed_idValue:
0x040a00a0
Identifier of the execute_write_completed event.
Definition at line
8808
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h