Data structure of the execute_write_completed event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_server_execute_write_completed_s::connection
Connection handle
Definition at line
8815
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
result#
uint16_t sl_bt_evt_gatt_server_execute_write_completed_s::result
Execute write result
Definition at line
8816
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h