Data structure of the subevent_tx_failed event.

Public Attributes#

uint8_t

Public Attribute Documentation#

advertising_set#

uint8_t sl_bt_evt_pawr_advertiser_subevent_tx_failed_s::advertising_set

The PAwR advertising set handle for the PAwR train that failed to transmit subevent data


Definition at line 5118 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

subevent#

uint8_t sl_bt_evt_pawr_advertiser_subevent_tx_failed_s::subevent

The subevent that failed to transmit subevent data


Definition at line 5120 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h