Utility Functions#
Utility functions for applications on SoC.
Functions#
sl_status_t
sl_btmesh_pop_event(sl_btmesh_msg_t *event)
bool
sl_btmesh_event_pending(void)
uint32_t
Function Documentation#
sl_btmesh_pop_event#
sl_status_t sl_btmesh_pop_event (sl_btmesh_msg_t * event)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_msg_t * | N/A | event | the pointer for storing the new event |
Get the next event that requires processing by user application. Application is not blocked if no event is waiting.
Returns
SL_STATUS_OK if a new event is returned, or SL_STATUS_NOT_FOUND if no event is waiting; other value indicates an error occurred
sl_btmesh_event_pending#
bool sl_btmesh_event_pending (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Check whether events are in queue pending for processing. Call sl_btmesh_pop_event to process pending events.
Returns
true if event is pending; false otherwise
sl_btmesh_event_pending_len#
uint32_t sl_btmesh_event_pending_len (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Check whether events are in queue pending for processing and return the next event length in bytes if events are pending. Call sl_btmesh_pop_event to process pending events.
Returns
the next event length if event is pending; 0 otherwise