Bluetooth Mesh Time Client Model#
Bluetooth Mesh Time Client Model.
This class provides the commands and messages to interface with the Time Client model
Modules#
sl_btmesh_evt_time_client_time_status
sl_btmesh_evt_time_client_time_zone_status
sl_btmesh_evt_time_client_tai_utc_delta_status
sl_btmesh_evt_time_client_time_role_status
Enumerations#
These values define the Time Role types used by the stack.
Functions#
Macros#
Enumeration Documentation#
sl_btmesh_time_client_time_roles_t#
sl_btmesh_time_client_time_roles_t
These values define the Time Role types used by the stack.
| Enumerator | |
|---|---|
| sl_btmesh_time_client_time_role_none | (0x0) The element does not participate in propagation of time information. |
| sl_btmesh_time_client_time_role_authority | (0x1) The element publishes Time Status messages but does not process received Time Status messages. |
| sl_btmesh_time_client_time_role_relay | (0x2) The element processes received and publishes Time Status messages. |
| sl_btmesh_time_client_time_role_client | (0x3) The element does not publish but processes received Time Status messages. |
Function Documentation#
sl_btmesh_time_client_init#
sl_status_t sl_btmesh_time_client_init (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
Initialize the Time Client model
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_time_client_deinit#
sl_status_t sl_btmesh_time_client_deinit (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
Deinitialize the Time Client model
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_time_client_get_time#
sl_status_t sl_btmesh_time_client_get_time (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | appkey_index | The application key index to use. |
Send a Time Get message to Time Server
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_time_client_set_time#
sl_status_t sl_btmesh_time_client_set_time (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, uint64_t tai_seconds, uint8_t subsecond, uint8_t uncertainty, uint8_t time_authority, int32_t tai_utc_delta, int16_t time_zone_offset)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | appkey_index | The application key index to use. |
| uint64_t | [in] | tai_seconds | The current TAI time in seconds since the epoch, 40-bit value |
| uint8_t | [in] | subsecond | The sub-second in units of 1/256th second. Range is 0-255. |
| uint8_t | [in] | uncertainty | The estimated uncertainty in 10-milliseconds steps. Range is 0-255, representing up to 2.55 seconds. |
| uint8_t | [in] | time_authority | 0: No Time Authority, the element does not have a trusted source of time such as GPS or NTP. 1: Time Authority, the element has a trusted source of time or a battery-backed properly initialized RTC. Other values are prohibited. |
| int32_t | [in] | tai_utc_delta | Current difference between TAI and UTC in seconds. Range is -255 to 32512. |
| int16_t | [in] | time_zone_offset | The local time zone offset in 15-minute increments. Range is -64 to 191, representing -16 to 47.75 hours. |
Send a Time Set message to Time Server
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_time_client_get_time_zone#
sl_status_t sl_btmesh_time_client_get_time_zone (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | appkey_index | The application key index to use. |
Send a Time Zone Get message to Time Server
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_time_client_set_time_zone#
sl_status_t sl_btmesh_time_client_set_time_zone (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, int16_t time_zone_offset_new, uint64_t tai_of_zone_change)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | appkey_index | The application key index to use. |
| int16_t | [in] | time_zone_offset_new | Upcoming local time zone offset. Range is -64 to 191, representing -16 to 47.75 hours. |
| uint64_t | [in] | tai_of_zone_change | TAI Seconds time of upcoming Time Zone offset change |
Send a Time Zone Set message to Time Server to set the Time Zone New state
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_time_client_get_tai_utc_delta#
sl_status_t sl_btmesh_time_client_get_tai_utc_delta (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | appkey_index | The application key index to use. |
Send a TAI-UTC Delta Get message to Time Server
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_time_client_set_tai_utc_delta#
sl_status_t sl_btmesh_time_client_set_tai_utc_delta (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, int32_t tai_utc_delta_new, uint64_t tai_of_delta_change)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | appkey_index | The application key index to use. |
| int32_t | [in] | tai_utc_delta_new | Upcoming difference between TAI and UTC is seconds. Range is -255 to 32512. |
| uint64_t | [in] | tai_of_delta_change | TAI Seconds time of the upcoming TAI-UTC Delta change |
Send a TAI-UTC Delta Set message to Time Server, which responds with a TAI-UTC Delta Status message.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_time_client_get_time_role#
sl_status_t sl_btmesh_time_client_get_time_role (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | appkey_index | The application key index to use. |
Send a Time Role Get message to Time Server, which responds with a Time Role Status message.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_time_client_set_time_role#
sl_status_t sl_btmesh_time_client_set_time_role (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, uint8_t time_role)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address |
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | appkey_index | The application key index to use. |
| uint8_t | [in] | time_role | The Time Role for the element. Range is 0 to 3.
|
Send Time Role Set message to Time Server, which responds with a Time Role Status message.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events