Bluetooth Mesh Sensor Server Model#

Bluetooth Mesh Sensor Server Model.

This class provides the commands and messages to interface with the Sensor Server model.

A Sensor State consists of four states:

  • Sensor Descriptor

  • Sensor Setting

  • Sensor Cadence

  • Measurement value

A multisensor setup is possible by having multiple sensor states within the same model, provided that each sensor has a unique Sensor Property ID.

Sensor Descriptor states are constant. Therefore, the stack can cache them and enumerate the present sensors to clients when requested.

Currently, the Sensor Server model does not cache the measurement data, sensor settings, or cadence. When a client is querying sensor data, the requests will be propagated to the application.

Modules#

sl_btmesh_evt_sensor_server_get_request

sl_btmesh_evt_sensor_server_get_column_request

sl_btmesh_evt_sensor_server_get_series_request

sl_btmesh_evt_sensor_server_publish

Functions#

sl_status_t
sl_btmesh_sensor_server_init(uint16_t elem_index, size_t descriptors_len, const uint8_t *descriptors)
sl_status_t
sl_btmesh_sensor_server_deinit(uint16_t elem_index)
sl_status_t
sl_btmesh_sensor_server_send_descriptor_status(uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, size_t descriptors_len, const uint8_t *descriptors)
sl_status_t
sl_btmesh_sensor_server_send_status(uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, size_t sensor_data_len, const uint8_t *sensor_data)
sl_status_t
sl_btmesh_sensor_server_send_column_status(uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, uint16_t property_id, size_t sensor_data_len, const uint8_t *sensor_data)
sl_status_t
sl_btmesh_sensor_server_send_series_status(uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, uint16_t property_id, size_t sensor_data_len, const uint8_t *sensor_data)

Function Documentation#

sl_btmesh_sensor_server_init#

sl_status_t sl_btmesh_sensor_server_init (uint16_t elem_index, size_t descriptors_len, const uint8_t * descriptors)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Server model element index

size_t[in]descriptors_len

Length of data in descriptors

const uint8_t *[in]descriptors

Sensor Descriptor State structures submitted as a byte array

A sensor descriptor represents the attributes describing the sensor data. It does not change throughout the lifetime of the element.

The following fields are required:

  • Sensor Property ID: 16 bits

  • Sensor Positive Tolerance: 12 bits

  • Sensor Negative Tolerance: 12 bits

  • Sensor Sampling Function: 8 bits

  • Sensor Measurement Period: 8 bits

  • Sensor Update Interval: 8 bits

Sensor Property ID is a 2-octet value referencing a device property that describes the meaning and the format of data reported by the sensor. The value 0x0000 is prohibited. Valid range is 0x0001 to 0xFFFF.

Initialize the Sensor Server model with Sensor Descriptors present at the element. The descriptors are cached and Descriptor Get queries are served without propagating it to the application. All incoming client queries are checked against the cached data. However, only valid requests related to existing sensors are propagated to the the application.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_sensor_server_deinit#

sl_status_t sl_btmesh_sensor_server_deinit (uint16_t elem_index)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Server model element index

Deinitialize the Sensor Server functionality. Note that the heap reserved space cannot be freed or reallocated. Reinitializing with greater number of sensors than before will eventually return an out of memory error until the device is reset.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_sensor_server_send_descriptor_status#

sl_status_t sl_btmesh_sensor_server_send_descriptor_status (uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, size_t descriptors_len, const uint8_t * descriptors)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]client_address

Destination client address. The address 0x0000 can be used to publish the message according to model configuration

uint16_t[in]elem_index

Server model element index

uint16_t[in]appkey_index

The application key index to use.

uint8_t[in]flags

No flags defined currently

size_t[in]descriptors_len

Length of data in descriptors

const uint8_t *[in]descriptors

Serialized Sensor Descriptor states for all sensors within the element consisting one or more 8 bytes structures as follows:

  • Sensor Property ID: 16 bits

  • Sensor Positive Tolerance: 12 bits

  • Sensor Negative Tolerance: 12 bits

  • Sensor Sampling Function: 8 bits

  • Sensor Measurement Period: 8 bits

Send a Descriptor Status message either as a reply to a Get Descriptor client request.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_sensor_server_send_status#

sl_status_t sl_btmesh_sensor_server_send_status (uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, size_t sensor_data_len, const uint8_t * sensor_data)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]client_address

Destination client address. The address 0x0000 can be used to publish the message according to model configuration

uint16_t[in]elem_index

Setup Server model element index

uint16_t[in]appkey_index

The application key index to use

uint8_t[in]flags

No flags defined currently

size_t[in]sensor_data_len

Length of data in sensor_data

const uint8_t *[in]sensor_data

Serialized Sensor Data consisting of one or more Sensor state for each sensor within the element. To simplify processing, the byte array is in TLV format:

  • 1st Property ID: 16 bits

  • Value Length: 8 bits

  • Value: variable

  • 2nd Property ID: 16 bits

  • Value Length: 8 bits

  • Value: variable

  • ...

If sensor data was requested for a Property ID that does not exist within the element, the reply must contain the given Property ID with zero length.

Send Sensor Status message as a reply to a Get client request or as an unsolicited message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_sensor_server_send_column_status#

sl_status_t sl_btmesh_sensor_server_send_column_status (uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, uint16_t property_id, size_t sensor_data_len, const uint8_t * sensor_data)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]client_address

Destination client address. The address 0x0000 can be used to publish the message according to model configuration

uint16_t[in]elem_index

Client model element index

uint16_t[in]appkey_index

The application key index to use.

uint8_t[in]flags

No flags defined currently

uint16_t[in]property_id

Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.

size_t[in]sensor_data_len

Length of data in sensor_data

const uint8_t *[in]sensor_data

Byte array containing the serialized Sensor Series Column state in the following format:

  • Sensor Raw Value X, variable length raw value representing the left corner of a column

  • Sensor Column Width, variable length raw value representing the width of the column

  • Sensor Raw Value Y, variable length raw value representing the height of the column

If the Property ID or the column ID (Raw value X) does not exist, the reply must contain only these two fields, omitting the optional Column Width and Raw Value Y fields.

Send Column Status message as a response to a Column Get client request or as an unsolicited message

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_sensor_server_send_series_status#

sl_status_t sl_btmesh_sensor_server_send_series_status (uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, uint16_t property_id, size_t sensor_data_len, const uint8_t * sensor_data)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]client_address

Destination client address. The address 0x0000 can be used to publish the message according to model configuration

uint16_t[in]elem_index

Client model element index

uint16_t[in]appkey_index

The application key index to use.

uint8_t[in]flags

No flags defined currently

uint16_t[in]property_id

Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.

size_t[in]sensor_data_len

Length of data in sensor_data

const uint8_t *[in]sensor_data

Byte array containing the serialized sequence of Sensor Series Column states in the following format:

  • 1st Sensor Raw Value X, variable length raw value representing the left corner of a column

  • 1st Sensor Column Width, variable length raw value representing the width of the column

  • 1st Sensor Raw Value Y, variable length raw value representing the height of the column

  • ...

  • Nth Sensor Raw Value X, variable length raw value representing the left corner of a column

  • Nth Sensor Column Width, variable length raw value representing the width of the column

  • Nth Sensor Raw Value Y, variable length raw value representing the height of the column

If Property ID does not exist in the element, the reply must contain only the given Property ID, omitting the other optional fields to column identifiers and column values.

Send Series Status message as a response to a Series Get client request or as an unsolicited message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Macro Definition Documentation#

sl_btmesh_cmd_sensor_server_init_id#

#define sl_btmesh_cmd_sensor_server_init_id
Value:
0x00470028

sl_btmesh_cmd_sensor_server_deinit_id#

#define sl_btmesh_cmd_sensor_server_deinit_id
Value:
0x01470028

sl_btmesh_cmd_sensor_server_send_descriptor_status_id#

#define sl_btmesh_cmd_sensor_server_send_descriptor_status_id
Value:
0x02470028

sl_btmesh_cmd_sensor_server_send_status_id#

#define sl_btmesh_cmd_sensor_server_send_status_id
Value:
0x03470028

sl_btmesh_cmd_sensor_server_send_column_status_id#

#define sl_btmesh_cmd_sensor_server_send_column_status_id
Value:
0x04470028

sl_btmesh_cmd_sensor_server_send_series_status_id#

#define sl_btmesh_cmd_sensor_server_send_series_status_id
Value:
0x05470028

sl_btmesh_rsp_sensor_server_init_id#

#define sl_btmesh_rsp_sensor_server_init_id
Value:
0x00470028

sl_btmesh_rsp_sensor_server_deinit_id#

#define sl_btmesh_rsp_sensor_server_deinit_id
Value:
0x01470028

sl_btmesh_rsp_sensor_server_send_descriptor_status_id#

#define sl_btmesh_rsp_sensor_server_send_descriptor_status_id
Value:
0x02470028

sl_btmesh_rsp_sensor_server_send_status_id#

#define sl_btmesh_rsp_sensor_server_send_status_id
Value:
0x03470028

sl_btmesh_rsp_sensor_server_send_column_status_id#

#define sl_btmesh_rsp_sensor_server_send_column_status_id
Value:
0x04470028

sl_btmesh_rsp_sensor_server_send_series_status_id#

#define sl_btmesh_rsp_sensor_server_send_series_status_id
Value:
0x05470028