Bluetooth Mesh Health Server Model#
Bluetooth Mesh Health Server Model.
This class provides the commands and messages to interface with the Health Server model
Modules#
sl_btmesh_evt_health_server_attention
sl_btmesh_evt_health_server_test_request
Functions#
Macros#
Function Documentation#
sl_btmesh_health_server_set_fault#
sl_status_t sl_btmesh_health_server_set_fault (uint16_t elem_index, uint8_t id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element on which the fault is occurring |
| uint8_t | [in] | id | Fault ID. See the Mesh Profile specification for IDs defined by the Bluetooth SIG. |
Set the fault condition on an element.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_health_server_clear_fault#
sl_status_t sl_btmesh_health_server_clear_fault (uint16_t elem_index, uint8_t id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element on which the fault is no longer occurring. |
| uint8_t | [in] | id | Fault ID. See the Mesh Profile specification for IDs defined by the Bluetooth SIG. |
Clear the fault condition on an element.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_health_server_send_test_response#
sl_status_t sl_btmesh_health_server_send_test_response (uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint16_t vendor_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | client_address | Address of the client model which sent the message |
| uint16_t | [in] | elem_index | Server model element index. Identifies the Server model that received the request as well as the element on which the test is to be performed. |
| uint16_t | [in] | appkey_index | The application key index to use in encrypting the request. |
| uint16_t | [in] | vendor_id | Bluetooth vendor ID used in the request |
Indicate to the stack that a test request has been completed and that the status may be communicated to the Health Client, which made the test request.
Returns
If an error occurs locally (for instance, because of invalid parameters), an errorcode parameter is returned immediately.