Bluetooth Mesh Light Control Server Model#
Bluetooth Mesh Light Control Server Model.
Bluetooth Mesh Light Control Server model functionality.
All LC Server state resides in and is own by the Model (stack). The state update notification events to the application are informational: the application is not required to react to them. The application may choose to save the LC Server state in persistent storage and set the states in the LC Server following a restart. To do this the application can utilize the notification events and update command.
Each LC Server instance requires that a Lightness Server is initialized in the element preceding the LC Server element: LC Server controls the Lightness Server residing in the preceding element. Each LC Server instance requires that a generic OnOff Server is initialized in the same element as the LC Server.
Modules#
sl_btmesh_evt_lc_server_mode_updated
sl_btmesh_evt_lc_server_om_updated
sl_btmesh_evt_lc_server_light_onoff_updated
sl_btmesh_evt_lc_server_occupancy_updated
sl_btmesh_evt_lc_server_ambient_lux_level_updated
sl_btmesh_evt_lc_server_linear_output_updated
sl_btmesh_evt_lc_server_state_updated
sl_btmesh_evt_lc_server_regulator_debug_info
Enumerations#
These values define the possible states of Light Controller.
These values identify optional diagnostic events that provide more information to the application about LC behavior.
Functions#
Macros#
Enumeration Documentation#
sl_btmesh_lc_server_lc_state_t#
sl_btmesh_lc_server_lc_state_t
These values define the possible states of Light Controller.
| Enumerator | |
|---|---|
| sl_btmesh_lc_server_lc_state_off | (0x0) The controller is turned off and does not control lighting. |
| sl_btmesh_lc_server_lc_state_standby | (0x1) The controller is turned on and awaits an event from an occupancy sensor or a manual switch. |
| sl_btmesh_lc_server_lc_state_fade_on | (0x2) The controller has been triggered and gradually transitions to the Run phase, gradually dimming the lights up.> |
| sl_btmesh_lc_server_lc_state_run | (0x3) The lights are on and the timer counts down (but may be re-triggered by a sensor or a switch event). |
| sl_btmesh_lc_server_lc_state_fade | (0x4) The Run timer has expired and the controller gradually transitions to the Prolong state. |
| sl_btmesh_lc_server_lc_state_prolong | (0x5) The lights are at a lower level and the timer counts down (but may be re-triggered by a sensor or a switch event). |
| sl_btmesh_lc_server_lc_state_fade_standby_auto | (0x6) The controller gradually returns to the Standby state |
| sl_btmesh_lc_server_lc_state_fade_standby_manual | (0x7) The controller gradually returns to the Standby state after external event. |
sl_btmesh_lc_server_lc_debug_events_t#
sl_btmesh_lc_server_lc_debug_events_t
These values identify optional diagnostic events that provide more information to the application about LC behavior.
| Enumerator | |
|---|---|
| sl_btmesh_lc_server_lc_event_state_updated | (0x1) Event reporting LC Server state machine state changes along with the remaining state timer. |
| sl_btmesh_lc_server_lc_event_regulator_debug_info | (0x2) Event reporting LC Server PI regulator integral term and regulator output. |
Function Documentation#
sl_btmesh_lc_server_init#
sl_status_t sl_btmesh_lc_server_init (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
Initialize the LC Server model. The server does not have any internal configuration. The command only activates the model in the mesh stack.
Each LC Server instance requires that a Lightness Server is initialized in the element preceding the LC Server element: LC Server controls the Lightness Server residing in the preceding element. Each LC Server instance requires that a generic OnOff Server is initialized in the same element as the LC Server.
LC properties are initialized as follows:
PropertyID: PropertyValue 0x002B: 0x111111, 0x002C: 0x011111, 0x002D: 0x001111, 0x002E: 0xf000, 0x002F: 0x0f00, 0x0030: 0x00f0, 0x031: 50, 0x032: 25.0, 0x0033: 250.0, 0x0034: 80.0, 0x0035: 80.0, 0x0036: 3000, 0x0037: 3000, 0x0038: 3000, 0x0039: 3000, 0x003A: 0, 0x003B: 3000, 0x003C: 3000
PI Regulator interval (T) is initialized to 50ms
The rest of the state values are initialized to zero
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_lc_server_deinit#
sl_status_t sl_btmesh_lc_server_deinit (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
De-initializes the LC Server model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_lc_server_update_mode#
sl_status_t sl_btmesh_lc_server_update_mode (uint16_t elem_index, uint8_t mode)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
| uint8_t | [in] | mode | Mode value. Valid range: 0-1. |
Update the LC Server model Mode state in the stack. Application may choose to directly set the model state in the stack, this function will pass the state value to the LC Server model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_lc_server_update_om#
sl_status_t sl_btmesh_lc_server_update_om (uint16_t elem_index, uint8_t om)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
| uint8_t | [in] | om | Occupancy Mode value. Valid range: 0-1. |
Update the LC Server model Occupancy Mode state in the stack. The application may choose to directly set the model state in the stack. This function will pass the state value to the LC Server model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_lc_server_update_light_onoff#
sl_status_t sl_btmesh_lc_server_update_light_onoff (uint16_t elem_index, uint8_t light_onoff, uint32_t transition_time_ms)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
| uint8_t | [in] | light_onoff | Light OnOff value. Valid range: 0-1. |
| uint32_t | [in] | transition_time_ms | Amount of time (in milliseconds) that the element will take to transition to the target state from the present state. If set to 0, the transition will be immediate. |
Update the LC Server model Light OnOff state in the stack. The application may choose to directly set the model state in the stack. This function will pass the state value to the LC Server model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_lc_server_init_all_properties#
sl_status_t sl_btmesh_lc_server_init_all_properties (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
Initialize all LC properties in one attempt. The following values are used:
PropertyID: PropertyValue 0x002B: 0x111111, 0x002C: 0x011111, 0x002D: 0x001111, 0x002E: 0xf000, 0x002F: 0x0f00, 0x0030: 0x00f0, 0x031: 50, 0x032: 25.0, 0x0033: 250.0, 0x0034: 80.0, 0x0035: 80.0, 0x0036: 3000, 0x0037: 3000, 0x0038: 3000, 0x0039: 3000, 0x003A: 0, 0x003B: 3000, 0x003C: 3000
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_lc_server_set_publish_mask#
sl_status_t sl_btmesh_lc_server_set_publish_mask (uint16_t elem_index, uint16_t status_type, uint8_t value)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
| uint16_t | [in] | status_type | The type of status message to turn on/off. Options for this are: LC Mode Status 0x8294 LC Occupancy Mode Status 0x8298 LC Light On Off Status 0x829C |
| uint8_t | [in] | value | Turn on or off the status message. Non zero - enable, otherwise disable. |
Update the bitmask that controls which messages are sent when the LC Server publishes. By default, the bitmask will be enabled to publish all three status messages.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_lc_server_set_regulator_interval#
sl_status_t sl_btmesh_lc_server_set_regulator_interval (uint16_t elem_index, uint8_t value)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
| uint8_t | [in] | value | Valid values are 1 ms-100 ms. (Default: 50 ms) |
Update the summation interval (T) at which the PI regulator is run. Only valid when the regulator is disabled (Light LC Mode is 0).
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_lc_server_set_event_mask#
sl_status_t sl_btmesh_lc_server_set_event_mask (uint16_t elem_index, uint16_t event_type, uint8_t value)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
| uint16_t | [in] | event_type | The type of event to enable/disable. Options are: lc_event_state_updated = 0x01, state_updated event report state changes lc_event_regulator_debug_info = 0x02, regulator_debug_info Regulator calculation details |
| uint8_t | [in] | value | Valid values are 0 and 1 to disable or enable the event |
Enable or disable additional diagnostics events. See lc_debug_events.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_lc_server_get_lc_state#
sl_status_t sl_btmesh_lc_server_get_lc_state (uint16_t elem_index, uint8_t * state, uint32_t * transition_time)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element. |
| uint8_t * | [out] | state | The current state of LC state machine |
| uint32_t * | [out] | transition_time | Transition time left for the current LC state. |
Fetch the current LC state. States can be as Off, Standby, Fade On, Run, Fade, Prolong, Fade Standby Auto, Fade Standby Manual
Returns
SL_STATUS_OK if successful. Error code otherwise.
Macro Definition Documentation#
sl_btmesh_cmd_lc_server_update_mode_id#
#define sl_btmesh_cmd_lc_server_update_mode_idValue:
0x024d0028
sl_btmesh_cmd_lc_server_update_light_onoff_id#
#define sl_btmesh_cmd_lc_server_update_light_onoff_idValue:
0x044d0028
sl_btmesh_cmd_lc_server_init_all_properties_id#
#define sl_btmesh_cmd_lc_server_init_all_properties_idValue:
0x054d0028
sl_btmesh_cmd_lc_server_set_publish_mask_id#
#define sl_btmesh_cmd_lc_server_set_publish_mask_idValue:
0x064d0028
sl_btmesh_cmd_lc_server_set_regulator_interval_id#
#define sl_btmesh_cmd_lc_server_set_regulator_interval_idValue:
0x074d0028
sl_btmesh_cmd_lc_server_set_event_mask_id#
#define sl_btmesh_cmd_lc_server_set_event_mask_idValue:
0x084d0028
sl_btmesh_cmd_lc_server_get_lc_state_id#
#define sl_btmesh_cmd_lc_server_get_lc_state_idValue:
0x094d0028
sl_btmesh_rsp_lc_server_update_mode_id#
#define sl_btmesh_rsp_lc_server_update_mode_idValue:
0x024d0028
sl_btmesh_rsp_lc_server_update_light_onoff_id#
#define sl_btmesh_rsp_lc_server_update_light_onoff_idValue:
0x044d0028
sl_btmesh_rsp_lc_server_init_all_properties_id#
#define sl_btmesh_rsp_lc_server_init_all_properties_idValue:
0x054d0028
sl_btmesh_rsp_lc_server_set_publish_mask_id#
#define sl_btmesh_rsp_lc_server_set_publish_mask_idValue:
0x064d0028
sl_btmesh_rsp_lc_server_set_regulator_interval_id#
#define sl_btmesh_rsp_lc_server_set_regulator_interval_idValue:
0x074d0028
sl_btmesh_rsp_lc_server_set_event_mask_id#
#define sl_btmesh_rsp_lc_server_set_event_mask_idValue:
0x084d0028
sl_btmesh_rsp_lc_server_get_lc_state_id#
#define sl_btmesh_rsp_lc_server_get_lc_state_idValue:
0x094d0028