Bluetooth Mesh Scheduler Server Model#
Bluetooth Mesh Scheduler Server Model.
This class provides commands and messages to interface with the Scheduler Server model
The scheduler server uses multiple fields to define the occurrence of an event and the type of event to be triggered. The field definitions are as follows.
Year
The year field represents 2 last significant digits of the year of the occurrence of the scheduled event.
0x00-0x63: 2 least significant digits of the year (0-99)
0x64: Any year
All other values are prohibited
Month
The month field represents the months of the occurrences of the scheduled event, using a bitfield with one bit for each month.
Bit 0: Scheduled in January
Bit 1: February
Bit 2: March
Bit 3: April
Bit 4: May
Bit 5: June
Bit 6: July
Bit 7: August
Bit 8: September
Bit 9: October
Bit 10: November
Bit 11: December
Day
The Day field represents the day of the month of the occurrence of the scheduled event. If the day of the month has a number that is larger than the number of days in the month, the event occurs in the last day of the month. For example, in February if the day field holds the value 29, the action is triggered on February 28th in a non-leap year or February 29th in a leap year.
0x00: Any day
0x01-0x1F: Day of the month (1-31)
All other values are prohibited
Hour
The Hour field represents the hour of the occurrence of the scheduled event.
0x00-0x17: Hour of the day (0-23)
0x18: Any hour of the day
0x19: Once a day (at a random hour)
All other values are prohibited
Minute
The Minute field represents the minute of the occurrence of the scheduled event.
0x00-0x3B: Minute of the hour (0-59)
0x3C: Any minute of the hour
0x3D: Every 15 minutes (0, 15, 30, 45)
0x3E: Every 20 minutes (0, 20, 40)
0x3F: Once an hour (at a random minute)
All other values are prohibited
Second
The Second field represents the second of the occurrence of the scheduled event.
0x00-0x3B: Seconds of the minute (0-59)
0x3C: Any second of the minute
0x3D: Every 15 seconds (0, 15, 30, 45)
0x3E: Every 20 seconds (0, 20, 40)
0x3F: Once a minute (at a random second)
All other values are prohibited
Day of Week
The DayOfWeek field represents the days of the week when the scheduled event will trigger. The week days are represented by a bitfield, by one bit for each day.
Bit 0: Scheduled on Mondays
Bit 1: Scheduled on Tuesdays
Bit 2: Scheduled on Wednesdays
Bit 3: Scheduled on Thursdays
Bit 4: Scheduled on Fridays
Bit 5: Scheduled on Saturdays
Bit 6: Scheduled on Sundays
Action
The action field represents an action to be executed for a scheduled event
0x00: Turn Off
0x01: Turn On
0x02: Scene Recall
0x0F: No action
All other values are prohibited
Transition time
This is a 1-octet value that consists of two fields: a 2-bit bit field representing the step resolution and a 6-bit bit field representing the number of transition steps.
Bit 0-1: Transition Step Resolution
0b00: The Default Transition Step Resolution is 100 milliseconds
0b01: 1 second resolution
0b10: 10 seconds resolution
0b11: 10 minutes resolution
Bit 2-7: Transition Number of Steps
0x00: The Transition Time is immediate
0x01-0x3E: The number of steps
0x3F: The value is unknown. The state cannot be set to this value, but an element may report an unknown value if a transition is higher than 0x3E or not determined
Modules#
sl_btmesh_evt_scheduler_server_action_changed
sl_btmesh_evt_scheduler_server_scene_changed
sl_btmesh_evt_scheduler_server_action_triggered
Functions#
Macros#
Function Documentation#
sl_btmesh_scheduler_server_init#
sl_status_t sl_btmesh_scheduler_server_init (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Scheduler server model element index |
Initialize the Scheduler Server model
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_scheduler_server_deinit#
sl_status_t sl_btmesh_scheduler_server_deinit (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Scheduler server model element index |
Deinitialize the Scheduler Server model
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_scheduler_server_get#
sl_status_t sl_btmesh_scheduler_server_get (uint16_t elem_index, uint16_t * status)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Scheduler server model element index |
| uint16_t * | [out] | status | Scheduler Server Scheduler Register status |
Get Scheduler Register status of Scheduler Server.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_scheduler_server_get_action#
sl_status_t sl_btmesh_scheduler_server_get_action (uint16_t elem_index, uint8_t index, uint8_t * index_, uint8_t * year, uint16_t * month, uint8_t * day, uint8_t * hour, uint8_t * minute, uint8_t * second, uint8_t * day_of_week, uint8_t * action, uint32_t * transition_time_ms, uint16_t * scene_number)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Scheduler server model element index |
| uint8_t | [in] | index | Index of the Scheduler Register entry to get |
| uint8_t * | [out] | index_ | Index of the Scheduler Register entry to set |
| uint8_t * | [out] | year | Scheduled year for the action |
| uint16_t * | [out] | month | Scheduled month for the action |
| uint8_t * | [out] | day | Scheduled day of the month for the action |
| uint8_t * | [out] | hour | Scheduled hour for the action |
| uint8_t * | [out] | minute | Scheduled minute for the action |
| uint8_t * | [out] | second | Scheduled second for the action |
| uint8_t * | [out] | day_of_week | Scheduled days of the week for the action |
| uint8_t * | [out] | action | Action to be performed at the scheduled time |
| uint32_t * | [out] | transition_time_ms | Transition time for this action |
| uint16_t * | [out] | scene_number | Scene number to be used for some actions |
Get the Scheduler Action defined by a Schedule Register state entry.
For the description of returned fields, see Scheduler Server
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_scheduler_server_set_action#
sl_status_t sl_btmesh_scheduler_server_set_action (uint16_t elem_index, uint8_t index, uint8_t year, uint16_t month, uint8_t day, uint8_t hour, uint8_t minute, uint8_t second, uint8_t day_of_week, uint8_t action, uint32_t transition_time_ms, uint16_t scene_number)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Scheduler server model element index |
| uint8_t | [in] | index | Index of the Scheduler Register entry to set |
| uint8_t | [in] | year | Scheduled year for the action |
| uint16_t | [in] | month | Scheduled month for the action |
| uint8_t | [in] | day | Scheduled day of the month for the action |
| uint8_t | [in] | hour | Scheduled hour for the action |
| uint8_t | [in] | minute | Scheduled minute for the action |
| uint8_t | [in] | second | Scheduled second for the action |
| uint8_t | [in] | day_of_week | Scheduled days of the week for the action |
| uint8_t | [in] | action | Action to be performed at the scheduled time |
| uint32_t | [in] | transition_time_ms | Transition time for this action |
| uint16_t | [in] | scene_number | Scene number to be used for some actions |
Set the given Scheduler Action entry of the Scheduler Register state.
For the description of these fields, see Scheduler Server
Returns
SL_STATUS_OK if successful. Error code otherwise.